Part Number: LP87524J-Q1 Other Parts Discussed in Thread: LMR23630-Q1 PN : LP87524JRNFTQ1
I'm inquiring.
Please check if the product above is mass-produced or a sample.
Thank you.
Hello,
CAD symbol is available here: http://www.ti.com/product/LP87524J-Q1/pinout-quality
You could take a look at http://www.ti.com/tool/mmwaveicboost which has LP87524J-Q1. Altium design files are available on that page.
Thanks.
Regards…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: LP87524-Q1 Tool/software: WEBENCH® Design Tools Hi,
I download PSpice model and try to use it to simulate on PSpice for TI. When I open simulation file, the tool show it is read only as the screenshot…
Part Number: LP87524J-Q1 Hi
My customer are doing short circuit test on LP87524J-Q1, schematics as below, after power on. They use a 30 cm cable connected at the top side of C26 to use the other end to touch the ground for doing short circuit test.…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: IWR6843 Hello, we have a board using the LP87524J-Q1 PMIC to drive an IWR6843 device. After power-up and when we read register PGOOD_FLT (0x2A), we get the value 0x01 indicating the PGOOD signal…
Part Number: LP87524J-Q1 I want to simulate the LP87524 power circuit. Is there any simulation software or library containing LP87524 chip? Is there any reference material for me to build models in other simulation software? Do you have any recommendations…
Part Number: LP87524J-Q1 Hi Team,
My customer now use LP87524J-Q1.
When power-up without any other configuration, customer found that buck 2 has no output and other's bucks are ok.
Buck0: 3.34V
Buck1:1.2V
Buck2:0V
Buck3:1.79V
May I ask why…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: IWR6843AOPEVM , IWR6843 ,
Team,
Customer is analyzing the IWR6843AOPEVM power consumption when the IWR6843 is kept in RESET.
It seems that a specific LP87524J-Q1 VIn value the current consumption…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: LP87524-Q1 Tool/software: WEBENCH® Design Tools Hi,
We would like to use LP87524 PSpice model LP87524-Q1_TRANS.LIB on TI TINA for SMPS simulation. We rename LP87524-Q1_TRANS.LIB as LP87524…