Part Number: LP87564-Q1 Hello TI team,
Please advise the minimum, Nominal ,maximum, and height tolerance of the device. Since this is not available on the datasheet.
P/N LP875640RNFRQ1
Part Number: LP87564-Q1 Hi team,
My customer cannot use 2MHz switching due to EMI test limit. This device can select the switching frequency from 2, 3 or 4MHz by OTP, right?
So I'd like to suggest them to select 3MHz switching. Can this device output…
Part Number: LP8764-Q1 Other Parts Discussed in Thread: LP87564-Q1 Hi Expert,
The customer will make the upgrade from LP87564-Q1 to LP8764-Q1 to has higher current rating.
I know there are not pin compatible.
And we want to know whether I2C command…
Part Number: LP87564-Q1 Hi Expert,
The deign adopted the LP87564-Q1.
And the output 1 is configured to 1V.
The condition:
The output voltage stay 1V at 0A.
Then switch to continuing 2A,the output become 0.75V continued,
We not found the…
Part Number: LP87564-Q1 Dear TI,
For one of our application we intend to use the LSF01 level shifters to convert an SDIo from 3V3 to 1V8. I saw in the logic minute that this device familly has a particular biasing circuit which requires the low level…
Part Number: LP87564-Q1 Can LP87564-Q1 slave address be changed through custom OTP setting? If not possible, I will recommend to use a I2C mux or use a separate bus.
Thanks, Alan
Part Number: LP87564-Q1 The LP87564 data sheet contains recommended inductors. I think, it is necessary to select the optimum inductor according to the output voltage and output current.
Can I use the recommended inductor(DFE252012PD-R47M or IHLP1616AB…
Other Parts Discussed in Thread: LP87564-Q1 , LP87561-Q1 , LP87565-Q1 , LP87562-Q1 , LP87563-Q1 , LP8756-Q1 This thread applies to LP87561-Q1, LP87562-Q1, LP87563-Q1, LP87564-Q1 and LP87565-Q1 devices.
LP8756x-Q1 devices have multiple different part…
Part Number: LP87564-Q1 Other Parts Discussed in Thread: LP8756-Q1 , TPS65400-Q1 Hello,
What are the default bootup voltages of LP87564?
Instead of requiring I2C programming or custom OTP spin, can the default bootup output voltages be configured…