Part Number: LP8764-Q1 Hi, Good day. Our customer is looking at the LP8764 and they have this question regarding the memory of this device: "We are interested in the new LP8764 PMIC. Unfortunately i did not understand how the programming of this PMIC will…
Part Number: LP8764-Q1 Hello,
Does the Rdson value mentioned in the LP8764-Q1 datasheet include metallization and package resistances?
Best regards,
Ahmed
Part Number: LP8764-Q1 Other Parts Discussed in Thread: LP87644Q1EVM Dear Support,
The LP8764-Q1 specification makes references to "Differential voltage sensing from point of the load"
Please advise how to do it?
Thanks,
Lauri
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: TPS6593-Q1 ,
This thread applies to TPS6593-Q1, TPS6594-Q1, LP8764, LP876x:
LDOVINT and LDOVRTC pins are externally accessible outputs for internal LDOs. It might be tempting to use these pins as…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: LP8764-Q1 , TPS6593-Q1 ,
This is relevant to TPS6593-Q1, TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices.
I2C addresses for your first device can be any valid value defined by the 7-Bit…
Part Number: LP8764-Q1 Dear Support,
The Automatic Phase adding and shedding option selection is supported for Buck 1 and Buck 3 in the PMICs GUI.
In case of automatic 2-phase configuration, which Bucks are they sharing the phase with?
I assume it is…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: LP8764-Q1
This is relevant to TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices:
The NVM programming on your PMIC can be confirmed by using the NVM Validation feature of the Scalable…
wang kun said: The FB of buck3 is grounded through 0ohm,is it possible that this problem is caused??
Yes, this is the cause of the problem. For this PDN, TPS65941213's FB3 pin is expecting 3.3V. Please see Note 9a in the PDN reference document.
-…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: LP8764-Q1 , TPS6593-Q1 ,
This is relevant to TPS6593-Q1, TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices:
The Real Time Clock function (RTC) provides a method by which the PMIC’s enabling…
Part Number: LP8764-Q1 In this version of the ECU, the mentioned part is used to power up the TDA2P we have the rails tied together for the TDA2P cores
I want TI to confirm if this would affect the TDA2P operation of the cores. Which values of the AVS…