Part Number: LP87745 Tool/software: Hello,
I am working on external watchdog implementation.
What will happen if I write value 0x00 to WD_ENABLE_REG when it's already '0' (I mean current value of WD_ENABLE_REG is zero already and we write the same…
Part Number: LP87745 Other Parts Discussed in Thread: AM2732 Tool/software: Hi All,
It is assumed that the AM2732 is used on its own, without IWR. In this case, should the recommended PMIC be LP87751A1? I don't understand what "y = platform" means.…
Part Number: LP87745-Q1 Other Parts Discussed in Thread: LP87745 last issue not been solved, so I repost it again.
We meet a issue on LP87745:
When install R261 to connect VIO to 3.3V (from 1 st BUCK), 5V output will down to 2.8V.
When uninstall…
Part Number: LP87745-Q1 Tool/software: Hello,
I'm working with LP87745-Q1 PMIC.
I want to use the watchdog of the PMIC and service it.
As far as I have seen, the Q&A watchdog must be serviced by sending answers in two different timing-windows…
Part Number: LP87745-Q1 Tool/software: Dear team,
Is there a way to force nINT output to high for LP877451-Q1(LP877451A4RXVRQ1 and LP877451LCRXVRQ1)? (Register configuration, etc.)
Details as below:
Current configuration: First set the watchdog…
Part Number: LP87745-Q1 Other Parts Discussed in Thread: LP877451Q1EVM Hello.
◎ I'm developing a radar sensor for vehicles. The components used are listed below, and the connection diagram can be found below.
AOP: AWR1843ARBGALPRQ1 BUCK: LM60430AQRPKRQ1…
Part Number: LP87745-Q1 Other Parts Discussed in Thread: AWR2944 , AWR2944EVM I have problem with the container of SBC in Davinci Configurator as the channel created in spi module as QSPI and I want it to be MIBSPI you can find the problem in attachment…
Part Number: LP87745-Q1 Other Parts Discussed in Thread: AWR2944 Tool/software: We are using the LP877451A1RXVRQ1 in our design. We found that the output voltage waveform in our design oscillated compared to the output voltage waveform of the AWR2944…
Part Number: LP87745-Q1
Tool/software:
Hi Expert,
Our product use LP87745 with AWR2944. The schematic is almost the same with AWR2944 EVM. one product (1 of 200pcs) LP87745 reported undervoltage when room teperature > 80℃。
We tested 1.8V voltage…