Part Number: LP8860-Q1 Hi team,
The LP8860-Q1 datasheet assumes the RISENSE=20mohm. However, can I use 25mohm (+/-5%) resistor at RISENSE? Could you tell me the relation ship between OCP current and register setting value with 25mohm?
Regards,
Nishim…
Part Number: LP8860-Q1
My customer is using LP8860-Q1 (D version) applied to AVN. There is currently a product with a problem with changing EEPROM Setting Data. LP8860-Q1 (Dversion) According to the application, there is no problem with mass production…
Part Number: LP8860-Q1 Other Parts Discussed in Thread: LP8866-Q1 , LM3424 Hello TI e2e team,
im design baclight driver card for multi displays
the VIn range is 14V to 35V
the output voltage change IAW the LEDs, 10 up to 100 with current of 100-400mA
i was…
Part Number: LP8860-Q1 Dear TI,
#HW information Mode : Display mode Brightness control : I2C BRT_MODE : Brightness register LED output : 3 (OUT1 ~ OUT3) voltage range : up to 29V LED current : 100mA
# EEPROM setting /* EEPROM code */ { 0x60, 0x0F, 0 }, {…
Part Number: LP8860-Q1 Other Parts Discussed in Thread: TLC59116-Q1 Hi,
My application requires controlling the brightness of four LEDs individually using I2C interface and PWM input. I find that LP8860-Q1 suits my application except that the boost regulator…
Part Number: LP8860-Q1 Other Parts Discussed in Thread: TPS61196-Q1 , LP8864S-Q1 hi,
I'm looking fora 8-ch booster (24Vin to 45Vout) with current sink, 150mA each.
I'm wondering if the LP8860 can be used in M/S topology (like the TPS61196-Q1): if…
Part Number: LP8860-Q1 Is there any possibility to disable the BL using the input VDDIO/EN and after that, the communication through SPI continues available?
According to figure 42, the device is in STANDBY or SHUTDOWN mode when VDDIO/EN = 0.
Thanks in…