Part Number: LP8862-Q1 Other Parts Discussed in Thread: LP8869-Q1 Hello,
Could you please help to provide the following information for the internal boost switch?
1) Rise Time 2) Fall Time 3) Body Diode Forward Voltage 4) Dead Time 5) Gate Charge…
Part Number: LP8862-Q1 Hi Team,
We have designed a schematic based on the LP8862-Q1 IC. Kindly review the attached schematic and share your feedback.
Let us know if any changes are required.
Regards,
Maishalini T
Part Number: LP8862-Q1 Hello,
I'm considering the LP8862-Q1. Another company has a similar product, the MAX16838. This product can also be used in combination with the MAX15054 high-side driver. Are there any products similar to the MAX15054 that can…
Part Number: LP8862-Q1 Tool/software: Hi,
I would like to know whether Output Voltage of driver can be paralleled with FET control to operate 2 different LED strings in which only one turns ON at a time.
5 LED's used in one String. Two strings has…
Part Number: LP8862-Q1 Other Parts Discussed in Thread: LP8867-Q1 Hi team,
Customer is wondering if they could lower the R2 to maybe 13K? And why d/s recommend such high value for R2?
Part Number: LP8862-Q1 HI TI!
I Have been designing a circuit for a LCD backlight driver using lp8862 .I 'm confused with the inductor selection part .
How can we determine the ripple current , is it 20-30% of inductor current?
Part Number: LP8862-Q1 Hi
Below is my customer schematics, would you help review the R302 and Q300 selection, are they good for 2MHz switching frequency ?
Part Number: LP8862-Q1 Hi
Would you help review my LP8862-Q1 SEPIC power stage design. does it make looks ok ?
Fullscreen
LP8862-Q1 SEPIC.txt
Download
SEPIC
4.5
36
23.8
0.3
2200
0.7
20
20
1
170
115
Part Number: LP8862-Q1
Hi
For the LP8862, is it feasible to have 2 LEDs on one channel and 3 LEDs on another channel? (in series)
We were thinking this would not be good, because the voltage would be too high for the 2-LED string and would cause…
Other Parts Discussed in Thread: TINA-TI , LP8862-Q1 hello Nikhil ,
I found the LP882-Q1 Spice Models can't be used in Tina, the error as below when I import that into TINA,