Part Number: LP8863-Q1
Our damage scenario is like this. At room temperature, turn on and off the IC repeatedly. The pressure test is repeated every 3 minutes. After 36 hours of cycling, it is found that the external MOS DS is short-circuited; Causes…
Part Number: LP8863-Q1 Hi Team
At present, it is found that the LP8863 will have insufficient vgs voltage driving force during the process of turning on the brightest and darkest to the steady state. Can you explain why the driving force of the red frame…
Part Number: LP8863-Q1 Hi team
I am looking for Spice model for LM61440AASQRJRRQ1&LP8863ADCPRQ1 (s-parameter or RLC SPICE file preferred).
Thanks
Stacy
Part Number: LP8863-Q1 Hello guys,
One of my customers is evaluating LP8863-Q1 for their next products.
At this moment, they have the following question about this device. Could you please give me your answer?
Q. According to the following comparison table…
Part Number: LP8863-Q1 Hi everyone,
i'm using the LP8863-Q1 in order to drive 6 led channels.
When an open led failure occurred i'm trying to clear the fault writing "1" in both status bit and clear bit the of interrupt_status2 register.…
Part Number: LP8863-Q1 Hi team,
My customer want to enable the low temperature limit function, could you help double check the setting.
step 1: set the low temperature limit
the register is oxEE, bit 0-8
what is the offset baseline, what is the actual…