Part Number: LP8863EVM Other Parts Discussed in Thread: LP8863-Q1 Hi there,
I'm currently testing the EVM board for the LP8863-Q1 driver.
I wondered whether there is an issue as the red LED D4 lights up (faintly) when I connect and turn on the LEDs…
Part Number: LP8863EVM
1. Is there a way to drive all the LEDs with an external power supply without using the boost feature at all?
2. How do I facilitate the SEPIC mode which caps the maximum voltage at 24V?
Many thanks,
Genevieve
Part Number: LP8863EVM My customer is requesting the Register Map file (.txt) with the POR-default register values that can be loaded in the LP8863EVM GUI. Can you provide this please? Thank you.
Part Number: LP8863EVM Hi all,
What is the meaning of "0h - MBB_region0_BX"?
When I change the 0h to 1h or 2h, the brightness going up, when I choose "6h-Fh - MBB_region0_BX", the brightness going back to original.
What is the meaning…
Part Number: LP8863EVM Other Parts Discussed in Thread: DS90UH928QEVM , , LP8863-Q1 , USB2ANY Hi TI Experts,
I am planning to use 2 of TI EVM's for my internal POC Project.
1. DS90UH928QEVM
2. LP8863EVM
Below is the block diagram of by Hardware set-up…
Part Number: LP8863EVM Hi TI Team,
I am doing an Internal POC where in i am considering to use LP8863EVM for controller the brightness of the Display.
I can see there is a software "setup_LP8863_EVM_1.0.0" which can be used to configure it. …
Part Number: LP8863EVM Other Parts Discussed in Thread: LP8863-Q1 Hello,
We have ordered a LP8863EVM, and just want to be 100% sure that we are operating it correctly and will not damage the unit.
As you can see, the spec sheet seems to have some conflicting…
Part Number: LP8863EVM Dears
I used LP8863EVM connect to 6S8P LEDs (LP8860-LEDLOADEVM) ,but LEDs havn't light
I was follow the Quick Start-Up Procedure described in User Guide
• Connect USB cable between EVB and PC
• Connect external power supply…