Part Number: LP8864-Q1 Tool/software: Hello Ti-Team, We have to design a controllable current source, which has to dim our high-power UV-LED analog.
The current should be regulated with the 12 Bit resolution. Our full scale current is 250mA. We would…
Part Number: LP8864S-Q1 Tool/software: Hi experts,
My customer Chery is using our LP8864S-Q1 on their Automotive display projects, could you please help provide the LP8864S-Q1 calculation tools for customer? Thanks!
Best regards,
Ankang
Part Number: LP8864S-Q1 Hi experts,
Chery is using our LP8864S-Q1 as their backlight driver on theri display project, need to confirm with you what the maximum value of Rg(the resistor on GD pin)? What's the effect will be caused by change the Rg…
Part Number: LP8864S-Q1 Tool/software: Hi team,
In LP8864S-Q1, there is booster mode and SEPIC mode, what is the difference? Can SEPIC mode work on both booster mode and buck mode?
for example, in my truck project, battery voltage is 24V typical(16V…
Part Number: LP8864-Q1 Hello E2E Experts,
Good day.
Is cascading 2 LP8864-Q1 to get more output channels possible?
Found a thread here:
LP8864-Q1: Power management forum
Regards,
Jonard
Part Number: LP8864S-Q1 Tool/software: LP8864 application circuit is as below, it is used as power supply for TFT panel backlight. When LP8864 EN pin is offered 3.3V, 948_VDD_BL_20.58V output 19.6V. But if PWM pin has 305Hz pwm signal input, the backlight…
Part Number: LP8864-Q1 Other Parts Discussed in Thread: LP8863-Q1
Tool/software:
Hi,
With an input voltage of 3.3V to 24V, approximately 20 LEDs are connected to the output stage. It is planned to be controlled by I2C and SPI, and a current of about…
Part Number: LP8864S-Q1 Other Parts Discussed in Thread: LP8860-Q1 Hi team,
Are there calculator tools for LP8860-Q1 and LP8864S-Q1 that can be provided to customers for design assistance? If so please help send it to me.