Part Number: LP8866S-Q1 Hi TI team,
In my current design, the input voltage 9~16V, target boost output voltage 35V, output current 810mA, switching frequency 400kHz, coil value 22uH.
Could you help recommend the Output Capacitor? Especially Electrolytic…
Hi Elbin,
Elbin Thomas said: The LP8873QRBBRQ1 seems to suit our requirements. However, the complete datasheet is not available on the website. Could you please share the full datasheet with us?
The datasheet and other materials can be requested through…
Part Number: LP8866-Q1 Hi team,
For the LP8866-Q1, is it possible for the LED_STATUS register (0x12) to read 0x0004?
This value corresponds to only LED3_FAULT (bit 2) = 1, while OPEN_LED (bit 6), SHORT_LED (bit 7), GND_LED (bit 8), and LED_STATUS…
Part Number: LP8866S-Q1 Other Parts Discussed in Thread: LP8866-Q1 Does the LP8866S-Q1 support ASIL-B functional safety? If the chip has no relevant certification, can it be used in ASIL-B compliant systems at the system level? Could you please provide…
Part Number: LP8866-Q1 Hi.
Datasheet for LP8866-Q1 lists the maxim output voltage as 48V (same as input voltage). What is the restriction on the output voltage?
We are looking to configure the LP8866 for 56-60V max output voltage (max current). Vin…
Part Number: LP8866-Q1 Dear TI experts,
My customer have a question about fault recovery of LP8866-Q1.
Section 6.3.9.4 of datasheet says about fault name and its action.
Some faults are enter fault recovery aumatically and some are not.
Do…
Part Number: LP8866-Q1 Hi Team,
We found Rev1 of "LP8866-Q1 BOOST LED Driver Design Tool" on a older E2E several years ago.
Customer is asking do we have newer version of LP8866-Q1 BOOST LED Driver Design Tool to share?
Thank you.
Tony
LP8866…