Part Number: LP8866S-Q1 Hi All
Right now i am checking the I2C Data result of LED Driver, using the I2C Reader tools, but when i got the result i cannot find the command of the write and read data on datasheet.
How to now what is the command or setting…
Part Number: LP8866S-Q1 Hi team,
My customer have question for 7.6.1.2 LED_CURR_CONFIG Register .
By this register setting, output current can reduce, does it? (e.g. 50 mA x FFFh(100%) = 50 mA)
Is there any precautions such as the duty being affected by…
Part Number: LP8866-Q1
Hi,
can I use the LP8866 in “ Direct PWM Mode ”
with external PWM of 60Hz and any ״PWM input minimum on time” that is greater than 200nSec?
Part Number: LP8866S-Q1 Hi Sir,
My customer has some questions about LP8866S-Q1, could it support the Luminous Intensity Minimum <2.5cd/㎡?
At this condition, the screen display does not have the jitters, flicker, or produce ripples or color casts. …
Part Number: LP8866S-Q1 Hi team,
The customer don't understand the set value of the output voltage.
In my understanding, they should set Vo = VF x n(LED#). Is it correct?
Or add voltage for condition fault monitoring?
Regards,
Youhei MIYAOKA
Part Number: LP8866S-Q1 Hi team,
I'd like to know the thermal information for LP8866SQRHBRQ1 (VQFN). There are only HTSSOP date in the datasheet. Could you please provid the thermal information of VQFN ?
Part Number: LP8866-Q1 Dear expert,
What does "internal short" status mean?
Customer project is already on mass production. They have one LP8866(black screen) register 0x12 report 0x1487. Does it mean LED 1,2,3 are all in "internal short" Status…
Part Number: LP8866-Q1 Hello ,
the datasheet and EVM both suggest that the electronic capacitors need to be placed between inductor and P-MOS, right?
if is possible to move to the input side, before the shunt resistor? How much impact does this design…