Part Number: LP8873-Q1 Other Parts Discussed in Thread: LP8870Q1EVM Dear TI Technical Support Team,
I am currently designing a dual-CCT LED desk lamp using two LP8873-Q1 devices (LP8873QPWPRQ1). Each LP8873-Q1 drives four LED strings, with one device…
Part Number: LP8873-Q1 I have a few questions regarding the LP8873-Q1 and would appreciate your guidance on the following points:
External 3.3 V Supply on VDD: If I am not using the internal LDO of the LP8873-Q1, can I directly provide an external…
Part Number: LP8873-Q1 hello Experts:
my use case : Voutmax=12*3.1=37.2V Iled=0.118mA/per channel*4=0.472mA
according to the equation from datasheet:
K L =0.5 fsw=400kHz
L=4*(37.2+0.5)/(27*0.472*0.5*400*1000)=59uH
Regarding inductor selection…
Part Number: LP8873-Q1 Hello TI team :
Application for our design LP8873 , combined all channle to one string with 8*LED current 230mA ,boost overvoltage limit is 35V , currently we are testing the LED- short to GND detetion function , get the result…
Part Number: LP8873-Q1 Dear TI,
I am looking for an automotive LED driver with Phase shift PWM. One of the components I came across was the LP8873-Q1. The price and relative simplicity (based on the amount of pins) has me interested. However, there…
Part Number: LP8873-Q1 Hello,
My customer is looking for an LED Driver IC that can support the LCD product of the specifications below.
- Manufacturer : BOE (LCD)
- Resolution : 7860 x 936
- Interface : DP 1.4 to eDP 1.4 (HBR3)
- Brightness…
Part Number: LP8873-Q1 Hello team:
We are testing LP8873 I2C on our HUD project (I2C communicate with MCU CYT2B93CAS), found a issue below show left side Pic with too long rise time for SCL and SDA , and SDA with two peaks ,
I modified the pull up…
Part Number: LP8866-Q1 Other Parts Discussed in Thread: LP8863-Q1 , LP8865Y-Q1 , LP8865Z-Q1 , LP8873-Q1 Hi Team,
I would like to know whether the LP8866QRHBRQ1 can be used to control two different types of LED sets independently. Also, can individual…
Part Number: LP8733-Q1 Hi team,
I'm BCCing my customer.
Regarding LP8873 XX RHDRQ1, I see that there are two TRMs for 4A and 42 variant
Could you tell me 00 and 44 variant OTP settings as well? Any format is okay, PDF is not mandatory. If you prefer…