Part Number: LSF0101 Hi team,
I would like to ask if I can use LSF0101 to transfer 1V to 1.8V?
It says "Allows bidirectional voltage-level translation between
0.95 V 1.8/2.5/3.3/5 V " in the datasheet.
in the Revision History, it says "Changed…
Part Number: LSF0101 Other Parts Discussed in Thread: SN74LVC2T45 , SN75LVDS387 , SN75LVDS386 , SN74LVC8T245 Hello TI team,
When I read the datasheet of the LSF0101, it seems that the current flowing to the I/O should be of the mA level (there are example…
Part Number: LSF0101 Hi Team,
Can you answer the following customer question please?
In our application I need a level shifter from 1.2V to 1.8V. According to the description this series should be suitable. But further down in the datasheet it says Vref_B…
Part Number: LSF0101 Other Parts Discussed in Thread: TXB0302 , TINA-TI Hi
I wish to simulate with LSF0101 PSPICE Transient Model in HSPICE (N-2017.12-SP2).
Please help with the documentation on connectivity and how to feed input stimulus.
Is there a user…
Part Number: LSF0101 Hello E2E,
What is the A1/B1 pin status while VREFA voltage drop to zero but VREFB and EN power is still given?
Any risk to damage IC at that abnormal condition?
~Jason
Part Number: LSF0101 Hi,
I want to use this component to interface my FPGA (1.8V) with external world.
The VCCA of the component would be 1.8V.
The VCCB would be 3.3V.
This configuration will work for sure.
But i want to keep the possibility to change…
Part Number: LSF0101 Greetings,
I will design a circuit that includes two voltage translators in series.
I have a SN74LVC1T45DBVR translator's output connected to the input of a LSF0101 voltage translator.
Are there any potential problems with interfacing…
Part Number: LSF0101 Is there a Spice model available for these parts?
If not, then is there a parameter set for the internal MOSFET so I could kludge my own?
My design has VREF_B at 3.3V. The other side will be varied by the application per the customer…
SDLS966L was a shared datasheet for LSF0101, LSF0102, and LSF0108. SDLS966M is available from the LSF0108 page.
The only changes in the datasheet are the upper limit in the recommended operating conditions (from 5 V to 5.5 V) and the thermal characteristics…
Part Number: LSF0101 Hi team,
Could you help solving following compile error when importing PSPICE to TINA?
"Invalid device: $CDNENCSTART. Line: #55."
Best regards,
Takeshi Sasaki