Part Number: LSF0204-Q1 Hi TI Team,
We are using LSF0204-Q in our circuit for level translating the 1.8V signal to 3.3V signal. The 1.8V supply is from a LDO and it is connected to the VREFA and 3.3V supply is connected to the VREFB. There is a pull…
Part Number: LSF0204-Q1 Other Parts Discussed in Thread: SN74LVC2G66-Q1 , TCA9517-Q1 , SN74LVC2G17-Q1 Can we use this part as buffer, by connecting Vref_A and Vref_B at the same voltage level?
Part Number: LSF0204-Q1 Other Parts Discussed in Thread: LSF0204 Team,
I'm surprised to not find more data on the saturation level of the input-output switch of this family of level shifters in the datasheet. from https://www.ti.com/lit/an/slva675b…
Part Number: LSF0204-Q1 Hi Ti team.
There is a regulation that the minimum operating voltage of Vref_B is Vref_A+0.8 V, but when the Vref_B side power down first, the regulation cannot be observed in the transient state.
In that case, is there a risk…
Part Number: LSF0204-Q1 Hello team,
My customer has one question double confirmed with you.
1. Up translation mode
At present, we do not add pull-up resistors on the low-voltage and high-voltage sides in this application. If it is an IO application…
Part Number: LSF0204-Q1 Hi,
I`m not pretty sure about it after reading the datasheet.
I have on side-B a voltage of 5V and on side-A a voltage of 1.8V. Do I need to use than 1.8V for the ENable pin or is 5V also fine?
As I`m coming from the uC…
Part Number: LSF0204-Q1
Hi guys,
I`m using the LSF0204QPWRQ1 for a downtranslation from 5V to 1.8V side.
Two pins are for I2C (B3, B4) and B1,B2 are GPIO-Pins coming from a uC 5V side.
The issue is I measure at Pin A1/A2 1.97V but the VREF_A…
Part Number: LSF0204-Q1 Hi Team,
I have read through some other e2e posts about the propagation delay on the LSF0204-Q1, but would like a bit more info.
A major concern with this part is the large range it shows for the propagation delay.
There…
Part Number: LSF0204-Q1 Hi BU team
Would you help double check whether application in figure 8-4 in the datasheet is right?
what's the VOL/VOH or VIL/VIH for B3/4 ?
what's the VOL/VOH or VIL/VIH for B1/2?
Thanks
Part Number: LSF0204-Q1 Hello, I am using the LSF0204-Q1 Levelshifter in my application.
1) Can the channels be operated independently in different directions at the same time (for example channel 1 from A to B and at the same time channel 2 from…