Part Number: LT1013 Hi,
I have two posts that In which they were resolved by your team. I want to delete both posts but there are no delete option.
Can you advise,
Thanks
Part Number: LT1013-DIE I have a customer troubleshooting a design that0 uses the TI LT1013-DIE. They are operating the amplifier in an non-inverting configuration with a gain of 2. They are experiencing distortion on the output at -55C. It resembles…
Other Parts Discussed in Thread: LT1013D , LT1013 Hi,
What is the output voltage swing range when the LT1013, LT1013A, LT1013D are operated at +-22V supply? Also what is the common-mode voltage range at this supply? Does the slew rate change from a…
Jib,
10mA is just a nice round easy to remember number. This current is considered safe for older junction isolated device like LT1013. Therefore no device damage will occur however the input current can cause unexpected results such as output inversion…
Other Parts Discussed in Thread: LT1013 Hi Ti people,
I would like to know if there is a specific failure mode of the LT1013 precision amplifier when applying a voltage over the absolute maximum ratings defined in the datasheet of this component.
…
Other Parts Discussed in Thread: LT1013 I'm using a TI LT1013 op-amp to process the current through a 50 mV shunt. I'm having some issues with the op-amp not performing well in certain conditions and I'm not sure why. It seems that the output of the opamp…
Part Number: LF353 Other Parts Discussed in Thread: MC1458 , PGA204 , LT1013 , LT1014 , LM211 , LP211 , LM239 , LM3302
[Case:710026]Technical Data Inquiry
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance…
Hi Mark,
Thank you for considering the LT1054. Figure 28 uses two 1N5817 diodes to replace the internal output stage switch legs in order to reverse the charge pump output polarity, and LT1013 is used for output error amplifier. By re-selecting the…
Hello Dimitri,
I am glad to hear that the LOG114 appears to be working to your expectations after making the op amp change. Modern chopper op amps can provide amazingly low voltage-offset and drift and high overall electrical performance, but they can…