Part Number: LT1054 Other Parts Discussed in Thread: TPS63700 Tool/software: Hi there.
I am looking to use the LT1054IDW soic16 package for its 5v to ±12 v application. Unless im totally missing somthing the "Figure 23. 5-V to ±12-V Converter" from…
Part Number: LT1054 Tool/software: Hi ,
I'm search the output -12V charge bump solution and ChatGPT suggest LT1054.
Do you have any other proposal ?
Vin has 3.3V/5V/12V can be optional.
Vout = -12V ; Iout = 10mA
Part Number: LT1054 My resolution:
I just had the same issue with startup of the LT1054, my load was an opamp and analog mux. < 55mA load
I had to wait > 30 seconds for a power cycle and even then, the LT1054 would latch at ~0.8V sometimes.
The…
Part Number: LT1054 Tool/software: Is this schematic design correct, Whether I will be able to get -12V at the output. Please let me know any updates to be added in design
Part Number: LT1054 Tool/software: Hi team,
we want to choose a device to against SGM3209, And customer need the operation temperature can above 85℃, could you help to provide a suitable device?
BR
Jingguo
Part Number: LT1054 Tool/software: Hi
We want to know the Vout voltage range of LT1054CDWR . In TI website it is mentioned as -1.25Vmin and -15V max for Vout. But in datasheet it is -4.7Vmin to -5.2Vmax.
we want to use this for a Vin of 5V and Vout…
Part Number: LT1054 Hello TI
We are planning to use LT1054IDW part in our design to generate -15V supply from +15V. We simulated the design with LTspice and could get the result as per requirement.
We would like to confirm this design configuration…
Part Number: LT1054 Other Parts Discussed in Thread: LM2660 , Tool/software: Hey Power Management Team,
I have a customer looking for a drop-in replacement for the ADI LT1054IS8#TRPBF and according to the TI BOM Cross Tool it shows that the TI LT1054IP…