Part Number: LV14540 Other Parts Discussed in Thread: TPS4800-Q1 , LM7480-Q1 , TPS4816-Q1 , LM74930-Q1 , Hi,
We are considering an input protection circuit for an automotive battery-powered product.
The downstream DC/DC converter is LV14540DDAR, and…
Part Number: LV14540 Hi,
I would like to confirm the function of the TI DC/DC converter shown in the subject.
Currently, we are considering an operation where VIN is always supplied (9 to 36 V), and the DC/DC output is controlled by turning the EN…
Part Number: LV14540 Hi,
I have a question regarding input voltage and input current noise in a power circuit using the LV14540DDAR.
We observe switching-synchronized noise superimposed on the input voltage and input current of the DC/DC converter…
Part Number: LV14540 Hi,
This is a continuation of the related questions.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1631356/lv14540-input-voltage-current-noise-synchronized-with-switching-operation…
Part Number: TPS54560 Other Parts Discussed in Thread: LV14540 , , LM76005 Hi,
I am currently considering a replacement for LV14540 and would like to ask for your advice.
As possible replacement candidates, I am considering the following two devices…
Part Number: LV14540 Other Parts Discussed in Thread: LM2679
I designed a 12V power supply around the LV14540 for a 3.5A load. The problem is that the load has a positive tempco so it is briefly much higher at startup. I can't get this to ever get out…
Part Number: LV14540 Hi,
We are using LV14540DDAR and observed a failure after an IEC ESD test. Please confirm if our understanding is correct and advise countermeasures.
ESD test / symptom
Standard: IEC 61000-4-2
Method: Contact discharge…
Part Number: LV14540 Hi,
We are evaluating a prototype board using LV14540DDAR and observed a failure during a system ESD test.
Test condition
IEC 61000-4-2 style ESD: ±8 kV contact discharge to the metal chassis/frame of the equipment (thermal…
Part Number: LV14540 Other Parts Discussed in Thread: LMR14050 Tool/software: I am trying to simulate a circuit using the LV14540 part number, but unfortunately, it is not available in Webench Power Designer. Could you please help me resolve this issue…