Part Number: LV2862 Other Parts Discussed in Thread: LM2611 Hi Team,
Could you pls check whether LV2862 support 12Vin to -12Vout/0.1A? Thanks
Regards, Hailiang
Hi, there.
I just got LMR16006X sample (instead of LV2862, because LMR16006X has better voltage accuracy(torelance) than LV2862),
and tested with 1000uF output capacitor.
Followings are waveforms. Ch1:VIN, Ch2:Vout(5V).
LMR16006X could start up with 1000uF…
Part Number: LV2862 Is the answer to the original question (linked to this one) correct? Unless I am missing something, according to SNVA856B the LV2862Y device should be able to operate as an Inverting Buck Boost (IBB), correct?
Part Number: LV2862 For the LV2862, what does it do if it is not operating (in SHDN or Vin absent) and you back feed power to the output?
For example, say LV2862 makes 5 volts from a higher voltage source. Another power supply makes 5.5 volts and diode…
Part Number: LV2862 Hello
Is it possibe to delete 100k resistor connecting to SHDN and VIN?
This means SHDN connect to VIN directly.
I do not use ON/OFF control using SHDN.
Part Number: LV2862 Hi Experts,
This device supports ECO mode. Customer wants to remove voltage ripple at light load.
1. Is it possible to disable ECO mode?
2. If not, what is the condition when device enters into ECO mode?
Regards,
uchikoshi
Part Number: LV2862 Hi ,
I have imported the PSpice model of LV2862XLVDDCR in my simulation tool, I am getting error. Can you please check and send the porper model.It would be very helpful for us.
Thank You.