Part Number: MAX232E Other Parts Discussed in Thread: MAX3232E Hi,
May I know the difference between MAX232E and MAX3232E?
Could they be replacement for each other?
Thanks and Best regards,
Tiger
Part Number: MAX232 Regarding unused pins, the following answer was given.
No; these logic inputs must not be allowed to float, so you need to connect them to VCC or GND.
7.3.2 of the datasheet states that there is a pull-up resistor.
I hear that there…
Part Number: MAX232E Other Parts Discussed in Thread: MAX3232E , MAX3232 Customer needs an IBIS model for the MAX232E.
We see that there is a model for the MAX3232E.
Is it accurate to use the MAX3232E IBIS model in leu of a model for the MAX232E?
If not…
Part Number: MAX232 Dear Team,
The customer is looking for a UART to RS232 IC, is this suitable? Does it need to convert the voltage again? Thank you
Many Thanks,
Jimmy
Part Number: MAX232E Hi,
My customer is planning to implement TMK107BJ105KA-T in C1, C2, C3 and C4 of the following circuit diagram.
Datasheet: https://html.alldatasheet.com/html-pdf/641924/TAIYO-YUDEN/TMK107BJ105KA-T/1474/2/TMK107BJ105KA-T.html
Can I…
Part Number: MAX232 Other Parts Discussed in Thread: TCA5405 , SN74LV8153 , TSU6111A , TCAL9539-Q1 Hey Interface team,
I have a customer working on a project and we were hoping to get your advice on possible solutions to a design challenge we are running…
Narendra,
We don't specify to comply with this standard - so we don't have the data and we will not collect it as this is not necessary for the vast majority of RS-232 applications.
Best,
Parker Dodson
Part Number: MAX232E Other Parts Discussed in Thread: TRS232E , , TRS202E Hello TI Experts,
The TRS232E SOIC (D) pkg is in EOL/LTB status, and the recommended replacement part is the MAX232E.
We have some boards in production for many years where the charge…
Part Number: MAX232E Hi TI team,
I am considering replacing the TRS232EIPWR with the MAX232EIPWR due to its EOL.
I compared the datasheets and found that the characteristics of those two ICs are the same. Are the TRS232EIPWR and MAX232EIPWR exactly the…