Part Number: MAX3222E Other Parts Discussed in Thread: MAX3221 Hi ,
Test the output signal of MAX3221 (V+, DIN1, DOUT1) and find the fluctuation, As shown in the figure, please help analyze it.Thanks!
Part Number: MAX3222E Hello Guys,
Good day.
Our customer is using MAX3222E with 3.3V Vcc. Due to some reasons they have to change VCC of MAX3222E to 5V. Will the output voltage VOH still be the same? Datasheet suggests that VOH = Vcc - 0.1 (typical…
Part Number: MAX3222 Hello E2E,
Our customer is evaluating MAX3222IPWR got after PCN for this device. The device befor PCN has not a step on output waveform, the device after PCN has a step on output.
Does TI know about this event? Does this event…
Part Number: MAX3222E Hi Team
Would you advise the rated current capacity of ROUT1 and ROUT2?
I couldn't find it in datasheet.
Thanks
Best regards,
Shidara
Part Number: TRS3222E Other Parts Discussed in Thread: MAX3222E , Hi Team,
what's the difference between TRS3222E & MAX3222E?
I compare the DS and they look like totally the same.
thanks a lot.
Best regards,
Yang
Part Number: MAX3222 Dear Sirs,
My customer asked us about tPHL,tPLH and tsk at Receiver Section of MAX3222.
In the specification table below, 1. Please let me know the min, max values of tPHL and tPLH. 2. Please let me know how to calculate the…
Part Number: MAX3222 Dear sir/madam,
In the datasheet of MAX3222 in section 8.2 Functional Block Diagram DIN is inverted to DOUT and RIN is inverted to ROUT.
Please explain why this inverting is done here? According to my understanding MAX3222, level…
Part Number: MAX3222 For the charge pump caps for V+/V- and C+/C-, is a tolerance of +/- 10% OK? If not, what is our recommended tolerance?
Best, Ishaan
Part Number: MAX3222 Hello,
Our customer use the MAX3222, have a question.
There are four capacitors for charge pump circuit.
How much the voltage rated for?
Could you give me the equivalent circuit of the charge pump?
Best Regards,
Naoki…