Other Parts Discussed in Thread: MAX3223 Hello,
Customer use MAX3223 and test supply current as below while auto power-down enable. But the 2.8mA have load looks large to customer. Do we have any comments or have lower supply current RS232 solution…
Other Parts Discussed in Thread: SN74LVC1G18 , MAX3223E kindly provide IBIS models for SN74LVC1G18 and MAX3223E because these two components are used in our design. My mail ID: venkatesh.ponduri@ananthtech.com
Hi Bitesh,
TRS3223E are functionally equivalent part replacements for the MAX3223E just as Clemens has stated.
I believe Bobby is contacting the marketing team to verify this matter. Please allow some time for the marketing team to process this request…
Other Parts Discussed in Thread: MAX3223 Hello,
Im implementing the circuit which is attached below with a MAX3223 and a Microcontroller. The pin FORCEON is controlled by a PIN of the Microcontroller. in order to manage te AUTOPOWERDOWN mode. The thing…
Other Parts Discussed in Thread: MAX3223 , MAX3232 Have several CCAs designed with Max3223 ICs powered with 3.3Vdc, all with 4 X 0.1uF external caps. None of them have we seen typical voltage level of 5.4V, per datasheet. Half of them we see less than min…
Other Parts Discussed in Thread: MAX3223 , MAX3223E Hello TI community,
On this occasion i'm here with the following enquiry: as you can see on the image attached i have a MAX3223 connection which i can't modificate and i need to looking the way to Disable…
Part Number: MAX3222E Other Parts Discussed in Thread: MAX3232 , MAX3223 , MAX3222 , Hi,
According to the 9.2 Typical Application in D/S, the RIN1 / 2 pull-down is outside the device. I think the MAX3232 and MAX3223 have a internal pull-down resistor, but…
Part Number: MSP430F6726A Other Parts Discussed in Thread: MAX3223 ,
Hi, Customers want to connect: MSP430F6726A(UART0 TX) --- MAX3223(DIN1)
They want to pull-up this signal line. Is there a recommended resistance value?
Customers want to add 1MΩ for reducing…