Part Number: MAX3232E Other Parts Discussed in Thread: TRS3232E , TRSF3232E Hi Team,
Can MAX3232E guaranteed 230kbps data rate? According to the data sheet, Max data rate is Min 150kbps and Typ 250kbps.
If the answer is no, I’m thinking of proposing TRS3232E…
Part Number: MAX3232E Other Parts Discussed in Thread: MAX3232 , Hi, TI expert
The figure below shows the serial port design of my MAX3232, The board is connected to the PC through the serial port cable A, and cable A is connected to the serial port to USB…
Part Number: MAX3232E-Q1 Hi,
Please tell me if there is a difference between MAX3232EIPWRQ1 and TRS3232EQPWRQ1 for the following information. I don't think I can disclose detailed information, so there is no problem to answer only Yes or No.
1. Die …
Part Number: MAX3232 Hello, I want to use the MAX3232 I.C. in order to use two different RS232 peripherals to communicate with a STM32 mcu. One of the peripherals has a baud rate of 9600Bps and the other has 115200Bps. Can I use both peripherals in the…
Part Number: MAX3232 Hello TI,
I am using MAX3232 RS-232 transceiver operated at 3.3V. I would like to use either 0.1uF,10%,0201,10V ceramic capacitor or 0.1uF,10%,0402,25V for C1-C4. My question is, the charge pump capacitor voltage can reach upto 6.6V…
Hi Parker, I have summarized responses to all of your above queries in the attached document. Please have a look. MAX3232E Debug.docx
After touch up, the DOUT voltage levels seem fine and I am not observing an junk on the serial console. However, I have…
Part Number: MAX232E Other Parts Discussed in Thread: MAX3232E Hi,
May I know the difference between MAX232E and MAX3232E?
Could they be replacement for each other?
Thanks and Best regards,
Tiger
Part Number: MAX3232 Hi,
I am using MAX3232 IC with a 3.3V supply. I would like to reduce impact of change pump ripple on my 3.3V supply since it is used to supply other devices on the board. I would like to add an LC filter at 3.3V supply line to suppress…
Part Number: MAX3232 Dear Team,
MPN MAX3232IDR, "13ADHKM" is marking on the IC body, may i know the meaning of this marking? is it Datacode 2023+ with lot number?
thank you.
Part Number: MAX3232 Other Parts Discussed in Thread: TRS3232E-Q1 Hello TI,
I am looking for major technical differences between below mentioned part numbers of RS-232 transceiver ICs. I could see only the operating temperature is different or am I overlooking…