Part Number: MC33063A Tool/software: Questions about MC33063A.pdf
I have a question about the VIpk of MC33063A.
I have written the details in a PDF file, so please answer.
Part Number: MC33063A-Q1 Tool/software: Hi
I am adding an external NPN BJT for an inverting circuit. While reviewing the datasheet, I noticed that Figure 7-7 on page 15 appears to be identical to Figure 7-4 , which seems unusual.
To address this,…
Part Number: MC33063A
For a current design with the DC DC converter MC33063ADR, there is being used an output capacitor of 1000uF with an ESR of 0.16 Ohms, and we are evaluating an alternate with the same specifications but with an ESR of 0.08, are…
Part Number: MC33063A Tool/software: Hi. I have a question about the MC33063A converter. We designed a buck converter 3V3@60mA and it worked well. However, we want to use the same controller to generate 3V3@150mA in the output. Our parameters is Vin …
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: MC33063A , LM51581 , LM5157 , LM5158 , TINA-TI Tool/software: Hi Team,
I have question about the switch current for the MC33063-Q1. Accouding to the datasheet, the switch current max value is…
Part Number: MC33063A Hi
I have a question: The picture below is the circuit in Spec.
1. Does this circuit use a switching frequency of KHz? ?
2 . For the CT mounted on Pin3-4, what is the basis for selecting 1500pF?
3. Formula table in Spec:…
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: MC33063A
Tool/software:
Hi. I have a question about the MC33063A converter. We are using R2 = 18K and R1 = 11K, with a desired Vout of 3.3V; however, we are getting 3.59V when Vin is 24V. The…
Part Number: MC33063A Dear Sir/Madam,
about MC33063ADR under PCN# 20230417002.1, Our customer, Sharp Malaysia, compared the output waveform of New Fab(RFAB) Sample and current Fab. (PCN Samples provided from TI Malaysia Sales as below. Sold/Ship to…
Part Number: MC33063A Hi,
I just want to confirm if I can use MC33063 for the conversion, Vin = 12V, Vout = -30V, 600mA. If not can you suggest any better devices.
Thanks,
Ranjini.R