Part Number: MC33063A Hello team,
I believe the max load is 1.5A for MC33063A.
Is there any minimum load requirement for MC33063A?
Best Regards,
Kei Kuwahara
Part Number: MC33063A I am using MC33063 in Step Down mode to achieve 5V, 700 mA from 24V VDC Input.
During the testing with Resistive load (e.g. No Load to 700 mA) continuous Humming Noise is listened.
I have conducted several tests to resolve this…
Part Number: MC33063A Tool/software: Some questions are as follows: 1. How is the output current derived in a boost circuit? 2. Are Q1 and Q2 in the step-down circuit a composite Darlington structure? 3. May I ask if the input voltage of a similar driving…
Part Number: MC33063A Other Parts Discussed in Thread: LM5157 , LM5122 Hi,
I want to use this component to design a step-up converter Vin=5V to Vout=24V. But there is also a situation when the input voltage is 24V. Can this component work good if input…
Part Number: TPS27081A Other Parts Discussed in Thread: MC33063A I saw such a circuit in the MC33063A datasheet for on/off operations, but do we need to do any pull-up or pull-down for ON/OFF?
Can I ON/OFF directly from the processor with 3.3V-0V without…
Part Number: MC33063A-Q1 Hi TI support team
I intend to use MC33063A-Q1 for 5V 200mA dc/dc regulator for a low orbit satellite circuitry. I assume the MC33063A-Q1 is fabricated with a BJT technology How can I verify that
Regards Shaya
Part Number: MC33063A Hai Sir,
Based on Customer recommendation we are using MC33063A for voltage conversion.
End application- Controlling & Analog outputs driving.
Can you please give me the clarification about my queries posted below...
1) Designing…
Part Number: MC33063A Other Parts Discussed in Thread: LM53603 Greetings,
I wanted to use MC33063A IC for bucking from 40V to 4V. The datasheet says "Switch Current Up to 1.5 A". My application would be to use this output to power up a few sensors,…