Hi Haroon,
Just for double check, oscillator frequency in the datasheet is the crossover frequency of MC33063A-Q1 ?
Customer mentioned Fco should be specified for this device, so please confirm if it's correct.
Part Number: MC33063A-Q1 Hi TI support team
I intend to use MC33063A-Q1 for 5V 200mA dc/dc regulator for a low orbit satellite circuitry. I assume the MC33063A-Q1 is fabricated with a BJT technology How can I verify that
Regards Shaya
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: MC33063A , ALLIGATOR Support,
I'm using an external P-chan FET for higher supply current. I worked through the formulas to determine my minimum inductance and output capacitance needed for my application…
Part Number: MC33063A-Q1 Support,
I think I may still be having issues with my supply! VOUT on the schematic is actually the +24V input. VFAN is +16V output to a fan. My Ct is currently 2200pF. My inductor current doesn't consistently go back to 0, as…
Part Number: MC33063A-Q1 Hello Team,
One of my customer want to understand behavior of MC33063A-Q1, when input voltage is greater than set output voltage in boost mode.
will it work in bypass mode?
is there any issue while operating in this region?
Regards…
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: TLV61048 Hi Team,
We have a customer who wants to use MC33063A-Q1 to step up the voltage from 5V to 12V at 0.5A output current. Can this device output 0.5A from a 5V input to 12V output? What would…
Part Number: MC33063A-Q1 Hi,
We are protecting input power against reverse polarity using P-Channel MOSFET. We referred multiple documents and ended up with confusions on Drain/Source connection. In some places the voltage input is connected to Drain…
Part Number: MC33063A-Q1 Other Parts Discussed in Thread: TPS61170 Hello,
For the part MC33063A-Q1, my input will be 5 V ? I want to achieve a boost output of 36V or higher. Is it achievable ?
This issue is related to ton,toff ratio. For a 36V output…