Part Number: MC34063A Hi team,
Does MC34063A can replace NCP3063 directly? PCB can not modify.
Some application Pin8 and Pin1 connect each other. Pin8 of NCP3063 is NC. thanks!
Part Number: MC34063A Other Parts Discussed in Thread: MC33063A , LM5157 Hello,
I would like to know if the MC34063A or the MC33063A can be used for the following step-up/boost converter applications?
Input Voltage Range 5-12V
Output Voltage: 14 or 1…
Part Number: MC34063A I am designing a 3.3VDC power supply using the MC34063A regulator. To mimimize part count on my board, I would like to use a 12.1K and 20K resistor to set the output voltage at 3.3V. I cannot find anything in the data sheet about…
Part Number: MC34063A Other Parts Discussed in Thread: LM5008 Hi,
I use MC34603 and LM5008 but meet EMI issue, I need provide what waveform to you for this issue?
Thanks
Jeff
Part Number: MC34063A Hi Expert,
Will need to design the MC34063A for Voltage-Inverting Converter Application. Need to define the ton/frequency firstly.
Pls advice whether the (figure 1 curve) for CT vs Ton/off will independent for varied Vin,Vo design…
Part Number: MC34063A We are planning to make a step up flyback using MC34063A. With the reference ckt given, can increase in turns ratio make output voltage go high ? And may i know how the feedback back works in the given reference schematic (i.e how…
Part Number: MC34063A Other Parts Discussed in Thread: TPS55340 , LM3478 Input is 12V, output I need is 12.6V with 1Amps current limit. Output connected: Lithium battery 8.1V to 12.6V range and a resistive load in parallel. Since battery is also connected…
Part Number: MC34063A Dear Representative,
we designed one DC-DC booster circuit with Vin 12V and output (V) :12.7V and current 275mA .
The below are the components used
Rcs 375E,
Rc 180E
R2: 20.33K
R1 2.2K
Li: 39UH Wruth Elelctronics
D1: 1N5819
Cf: 2…
Part Number: MC34063A
Hello everyone,
I am working with a MC34063A voltage regulator in order to prototype step-up power management solution, with control logic to switch between three different output values. I encountered some issues while trying to…