Part Number: MCF8315C-Q1 Other Parts Discussed in Thread: MCF8315C Our customer uses MCF8315C‑Q1 for automotive AGS (Active Grille Shutter), which requires accurate position control.
As the device only provides sensor‑less FOC speed closed‑loop, position…
Part Number: MCF8315C Other Parts Discussed in Thread: MCF8315D Dear FAE,
Prompt 'CONTROLLER_FAULT', 'MPET_BEMF_FAULT',When use motor studio smart tune. However motor can spin about 5 second when 'Configuration'
Motor Parameter:
Driver Volatge …
Part Number: MCF8315C
My name is Uechi from Tenryu Marusawa Co., Ltd. in Japan.
I have selected your MCF8315C for a circuit design project, but I am struggling due to an insufficient understanding of the specifications.
Regarding the I2C communication…
Part Number: MCF8315C Other Parts Discussed in Thread: MOTORSTUDIO Tool/software: Dear Sir,
I was testing the fan using TI GUI version 1.30 . When I ran the fan at 400 RPM , I observed that the bus current increased significantly , but the three-phase…
Part Number: MCF8315C Hi support team all.
- What are the disadvantages of setting PWM_FREQ_OUT to a high value (60 kHz)?
- What are the expected advantages of enabling DINAMIC_CSA_ GAIN? What are the disadvantages?
Best regards,
DH
Part Number: MCF8315A After replacing the damaged MCF8315A IC on the MCF8315A EVM board with a new device, the hardware appears to be functioning correctly. All the required supply voltages, including AVDD , BUCK , and DVDD , are present and within the…
Part Number: MCF8315C In ISD_CONFID register there is one name BRK_MODE which represent the mode of brake. Here two option available where 0b represent reserved bit. What does that mean. If I select the BRK_MODE as 0b make the active motor disable ?
Part Number: MCF8315C Tool/software: I want to use an external microcontroller to control the MCF8315C controller. Is there a driver library available where all the registers and variables are defined?
Part Number: MCF8315C In ISD_CONFID register there is one name BRK_MODE which represent the mode of brake. Here two option available where 0b represent reserved bit. What does that mean. If I select the BRK_MODE as 0b make the active motor disable ?
Part Number: MCF8315PWPEVM Other Parts Discussed in Thread: MOTORSTUDIO I've purchased a 2nd evaluation board to build a 2nd test rig, the first I setup with MotorStudio, and wrote an embedded driver to communicate without a problem however this second…