Part Number: MCF8316D I have a board where I want to enable both on internal MFC8316 based motor driver and also enable an external motor driver module. If I float VM, or tie lightly to gnd, can I leave the motor driver and i2c ports connected to the…
Part Number: MCF8316D Other Parts Discussed in Thread: MCF8329A , MCF8329HS , CSD18532Q5B Hi Team TI, We are planning to use two motor drivers in our application to drive 6S and 12S BLDC motors. We have shortlisted MCF8316DVRGF and MCF8329A1IREER both…
Part Number: MCF8316D
We are currently evaluating the adoption of the TI BLDC motor driver MCF8316D . We have obtained the evaluation module MCF8316DEVM and are in the process of verifying its operation by connecting a BLDC motor available to us.
…
Part Number: MCF8316D Hello! I'd like to ask if the Device ID of this chip is locked! The problem is as follows:
1. I unsoldered the MCF8316D EVB-adjusted chip and soldered it to a self-made board for I2C programming. Reading and writing were fine.…
Part Number: MCF8316D Other Parts Discussed in Thread: MCF8315D , MCF8329HS , MCF8315C MCF8316D datasheet §7.5.1 states: “Whenever DRVOFF is driven high, it should be held high for a minimum of 10s for safe operation.”
Could TI please clarify the reason…
Part Number: MCF8316D Other Parts Discussed in Thread: MOTORSTUDIO , MCF8329HS Hi,
I'm trying to tune a MCF8316D driver with a LS-7060 DC Centrifugal Brushless Air Blower motor. The datasheet is attached.
LS7060.pdf
I'm using motor studio with the…
Part Number: MCF8316D Other Parts Discussed in Thread: MCT8316Z , Hi e2e team,
I'm looking to use a motor driver in a system that uses a belt drive to move a heavy load (several kg) back and forth. I was previously considering the
MCT8316Z, but I…
Part Number: MCF8316D Hello Experts,
is it possible for the MCF8316D to survive a higher voltage than 40 V during the 8/20 us surge pulse test (IEC 61000-4-5). Could it handle up to 60 V during this test?
Regards,
Armin
Part Number: MCF8316D-Q1 Other Parts Discussed in Thread: MCF8316D Dear TI experts,
My customer want to use mCF8316D-Q1 for their next project.
The project is Active air flap in front of the car like below.
As you see it is very important to detect…
Part Number: MCF8316D
Hey team/fellow engineers.
I am attempting to build my own board using the MCF8316D. Unfortunately the board's digital portion doesn't seem to be working properly. I can tell this because I can't get any voltage out of DVDD and…