Part Number: MCF8329A Hi
I am using GUI version 0.1.15.
EVM board and GUI art not connecting.
Looking at Device Manager, the USB driver is no installed.
Please share usb driver to connect EVM board to PC.
Regards.
Hi Joshua-san
Unfortunately, my customer was unable to complete the system by the deadline and changed their mind to an alternative method.
I appreciate for your kind support.
I will close this thread.
Best regards,
Higa
Part Number: MCF8316A Other Parts Discussed in Thread: MCF8329A
I have the following HW setup:
1. MCF8316A EVM
2. Maxon 449464 motor
3. 24V 3A bench power supply
Default registers preset loaded using Motor Studio and then MPET runs successfully with 60…
Part Number: MCF8329A Hi support team.
I have a inquiry regarding BUS CURRENT resister.
I use EVM to adjust the motor rotation.
Therefore, I am monitoring the BUS_CURRENT register (40Eh), which is a read-only register of the device, but the value remains…
Part Number: MCF8329A The sensorless FOC control algorithm needs to know the BLDC motor coil resistance, inductance, and the motor's BEMF constant, in order to calculate the rotor position. With what level of accuracy does each of these parameters…
Part Number: MCF8329A Other Parts Discussed in Thread: MCF8329EVM , MCF8316A I'm testing the MCF8329EVM in an application with pretty high load that engages quickly and often getting LOCK_ILIMIT faults. My motor is rated for peak currents of 78A, my BASE_CURRENT…
Hello TI experts,
As I see in this presentation , on page 4, MCF8329 is a future roadmap product. Could you please advise expected timelines on when samples and evaluation board will be available?
How can we get early access to the evaluation board or…
Hi Babji,
Babji Bommana said: Can I use multiple parallel MOSFETs to achieve the desired current ratings, or is there something else I should consider changing?
There should not be an issue with using parallel MOSFETs.
I would recommend taking a look at…
Part Number: MCF8315A Other Parts Discussed in Thread: MCF8315EVM , , MCF8329A , MCF8316A Tool/software: Hi team,
May I ask why the customer cannot choose the Brake_pin_mode based on the MCF8315EVM?(They choose device MCF8315A)
But when they choose the device…
Hi Eric,
Motor studio today supports, MCF8316A, MCF8316C, MCF8315A, MCF8315C, MCF8329A, all FOC devices. Future releases will be planned for MCT831x, MCT8329 devices.
MCF831x do not support lead angle as they are meant for non salient motors where LD…