Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A , LVBLDCMTR , MOTORSTUDIO Tool/software: Hi
I recently bought an MCF8329EVM and I have been trying to set it up to spin my motor.
I have not been able to get the SmartTune or MPET tools…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A , MOTORSTUDIO Tool/software: First off. My PCB looks different than in the instructions. I can't find SW1, and some other minor differences. It says MD098A-001 on it. Not sure if this is…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A Tool/software: I am trying to run a motor with motor studio and MCF8329A. I load the BLDC Pump 3A json file. When I run the MPET with Run MPET the motor starts rotating after some delay…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A Tool/software: I am working with a 24V, 250W, 3000RPM Brushless DC motor( Model: RMCS-1035) using the MCP8329EVM board. I tried using the default JSON file provided in the TI support reply…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A 이 보드로 BLDC모터를 제어하려고 하는데 첨부한 사진과 같이 MPET RESULT를 보면 Resistance 및 inductance 값을 기입할때 모터의 상저항인지 선간저항인지,
inductance는 모터 코일의 인덕턴스인지,모터 자체의 인덕 턴스인지 혹은 모터의 무부하 인덕턴스 값 중 어느값을 넣어서 모터를 돌려야 하는지…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A , MOTORSTUDIO Tool/software: The Base Current I calculated using the Equation given in the MCF8329A Tuning guide (with RSENSE=1mOhm; CSA_GAIN=40 V/V as that was the value in the corresponding…
Part Number: MCF8329EVM Other Parts Discussed in Thread: MCF8329A-Q1 , MCF8329RRYEVM , MOTORSTUDIO , MCF8329A ,
Tool/software:
Hello TI-Team,
we are developing an automotive part and thus we need the MCF8329A-Q1. However for evaluation I an wondering…
Part Number: MCF8329EVM Tool/software: I got a mcf8329evm board today.
It connected to motor studio successfully.
But MPET is not operated properly. several fault occurred.
CONTROLLER_FAULT, MPET_BEMF_FAULT.
my motor does not spin in MPET mode…
Part Number: MCF8329EVM Tool/software: Hi team,
My cuatomer use MCF8329EVM to do some test.
The product is Pump and spec is 48V@400W
But some question below,
1. The fan does not start smoothly, it makes a clicking sound and starts intermittently…