Part Number: MCF8329HS-Q1 Hello,
I recently started using power control mode on the MCF8329HS-Q1 chip. I set the power to slightly more than I expect for my application, then set the max speed to where I want the motor to run. I mainly did this to make…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329HS
Dear TI experts,
My customer made their schematic using MCF8329HS-Q1 for 48V battery system.
Could you review this schematic?
MCF8329HS-Q1_sch.pdf
And one more request, please…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MOTORSTUDIO Dear TI experts,
My customer want to connect their custom PCB to MotorStudio to set the parameter through EVM.
In this case, which pins should I connect to EVM except SCL, SDA…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329HS Dear TI experts,
My customer have question about MCF8329HS-Q1. Could you check it?
About dead time, 1000ns is maximum value? Can I set to 200ns?
2. I cannot find "Dead time…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329HS , MCF8329A Hello TI Team,
I am contacting behalf of the DURA Automotive systems. we have few questions regarding the operation/interface with the MCF8329HS-Q1 IC. We are planning to…
Part Number: MCF8329HS-Q1 Dear TI experts,
My customer send me a question about the value of shunt resistor.
Now they applied 3 MCF8329HS-Q1 in one PCB.
one is for 12V/35A cooling fan, and 2 are for 12V/6.5A EWP.
I suggested 1mohm shunt resistor…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329HSRRYEVM , MCF8329A-Q1 , MCF8329HS , MSP430FR2355 , MOTORSTUDIO , Hello,
My customer has been struggling on EEPROM write operation on MCF8329HSRRYEVM. Would you please give me your comments…
Part Number: MCF8329HS-Q1 Dear TI experts,
My customer prepare to test MCF8329HS-Q1 EVM based on 48V battery input.
I think MCF8329HS-Q1 itself is okay because its Vin is up to 65V, but other devices are not sure that it is right to test 48V battery…
Part Number: MCF8329HS-Q1 Dear TI experts,
Could you explain the difference between ISD_SPEED and FG_SPEED_FDBK?
I think these 2 registers are about measuring motor speed, but I cannot see specific differences.
and,
If these 2 registers are…
Part Number: MCF8329HS-Q1 Other Parts Discussed in Thread: MCF8329A-Q1 , Dear TI experts,
Could you check that the offsets of GATE_DRIVER_FAULT_STATUS is 0h and CONTROLLER_FAULT_STATUS is 2h?
I am asking it because if my customer read this offset…