Hi Shachar,
The value in DC_BUS_CURRENT will give you the current being pulled from the VM input. This value should be reasonably accurate with its resolution being limited by the total available bits.
The functionality of the DC_BUS_CURRENT bit field…
Hi Lien,
Lien Tori said: Is there any issue if the 3.3V goes up 1 sec after the main power? Because in some cases we are experimenting that, and the MCT doesn´t answer
If this 3.3V source is being used to pull up FG and nFAULT, then the 3.3V coming up…
Part Number: MCT8315A Tool/software:
See picture,this is Open-loop to Closed-loop Conversion oscilloscope waveform,my motor startup failure at this moment.
I need some advice how to optimize this waveform,Make this electromagnetic Angle accurate.
…
Part Number: MCT8315A Tool/software: Hi,
I use a MTC8315AIV on a custom board and I have a strange behavior when I configure EEPROM register TRAP_CONFIG1 .
According to the datasheed the bit 19 of TRAP_CONFIG1 is reserved and I would expect that its…
Part Number: MCT8315A Other Parts Discussed in Thread: MCF8316A Tool/software: Hi,
I use a MTC8315AIV on a custom board, and I have an issue about I2C (no response of MCT). I make a long time to isolate the problem, but now I have only one parameter …
Part Number: MCT8316A Other Parts Discussed in Thread: MCT8315A Tool/software: Hi there,
We intend to use MCT8316A and MCT8315A in the design.
We don't need to use the SW_BK (internal Step-Down Back regulator) option.
My question is, can I remove…
Part Number: MCT8315A Tool/software: Hello team,
1. My customer is looking for quickest way to stop the rotating motor. What is the recommended method?
2. What are BRAKE_EN and STAT_BRK_EN for? My customer was able to stop the motor by writing BRAKE_INPUT…
Part Number: MCT8315A Tool/software: Hello team,
What should I do, if I am not using EXT_CLK and EXT_WD?
Should I leave them floating or connect to GND?
Best Regards, Kei Kuwahara