Part Number: MCT8316A Other Parts Discussed in Thread: MSP430FR2355 We are currently using the STM32H7 series chips to communicate with the MCT8316A chip, and at the same time, we want to use MCT8316GUI to debug the MCT8316A chip. However, when opening…
Part Number: MCT8316A Subject: MCT8316A Transition Issue from Open-Loop to Closed-Loop at Low Temperatures
System Overview:
Motor: 3-phase Brushless DC (BLDC) motor
Specs: ~25W rated power, 12 pole pairs
Driver: MCT8316A
Target…
Part Number: MCT8316A-Q1 Other Parts Discussed in Thread: MCF8316A-Q1 Dear TI experts,
My customer now test MCF8316A-Q1 in their own PCB.
During the test they found that motor is not running in specific situation.
Vin=12V, Current=nomal 1A under…
Part Number: MCT8316A Other Parts Discussed in Thread: MCF8316D , MOTORSTUDIO If I purchase MCT8316AT, will it operate even if I input a PWM signal to the SPEED/WAKE pin? If it will operate, which pins should I configure and how should I configure them…
Part Number: MCT8316A-Q1 Other Parts Discussed in Thread: MCF8316D , MCF8316C-Q1 , MCT8316A
Dear TI experts,
My customer made their schematic using MCT8316A1VQRGFRQ1. Could you review this schematic?
(Schematic is deleted due to customer's request…
Part Number: MCT8316A Other Parts Discussed in Thread: MCF8315C , , MCF8315D , MOTORSTUDIO Dear Support,
I have been integrating a bidirectional motor control using MCF8315C (Integrated FOC driver). I have been having an issue that the driver get very…
Part Number: MCT8316A-Q1 Hi TI team,
This is a follow up of this
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1639016/mct8316a-q1-i2c-bus-recovery-and-internal-reset-logic
Unfortunately, even though we have…
Part Number: MCT8316A Tool/software: Hi,
We just got the second layout of the board which having 3 MCT8316A IC's on board
The 1st board was for evaluation only, the 2nd round is the 1st operational layout candidate
There is minor circuit change…
Part Number: MCT8316A Tool/software: Hi Sir :
Our application scenario is to use MCU and this chip to control the rod motor. Regarding this chip, I have a few questions to ask: 1. Does this driver chip only support automatic control? If we only want…