Part Number: MCT8316AEVM Dear Technical Support, Good day! Please verify for MCT8316AEVM and provide guidance for proper operation. Or confirm if can be considered as defective ? I connected a 12V power supply and wired the brushless motor. After turning…
Part Number: MCT8316AEVM I'm currently working on the MCT8316AEVM and I was trying to understand the data from the DACOUT pins, I see that there are quite a number of varaibles we can monitor on them. I wanted descriptions on the parameters measured like…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A I'm currently working on the MCT8316AEVM and I was trying to understand the data from the DACOUT pins, I see that there are quite a number of varaibles we can monitor on them. I wanted…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A I'm using a A2212/6T/2200V bldc motor, I'm trying to calculate the efficiency of it, which I'm getting to be 30.07%. My input ratings are 12V @ 0.15A so power is 1.815W, and output power…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MSP430FR2355 , MCT8315A , MCT8316A Hi!
Hi! I'm using MCT8316AEVM to experiment with MCT8316A1V.
It was told to me that MCT8316A1V's I2C interface does not support clock stretching, but the…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MSP430FR2355 , UNIFLASH , MCT8316A Tool/software: From the Link which you've provided i was able to download the firmware for the 8316A, BTW still not fixed in the download page. But after flashing…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A , MSP430FR2355 , MCF8316AEVM , MCT8315A Hi TI Team,
We are using the MCT8316A EVM and need to write a custom script outside of the standard GUI that turns on the motor and polls status…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MSP430FR2355 Hi! While using the MCT8316AEVM to experiment with the MCT8316A1V, I captured the following I2C frame using the logic analyzer.
As can be seen, the MSP430FR2355's SCL line 'freezes…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MSP430FR2355 , MCT8316A , MCT8315A Hi! While using the MCT8316AEVM to experiment with the MCT8316A1V, I captured the following I2C frame using the logic analyzer.
As can be seen, the MSP430FR2355…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A , MCT8329A , MCF8329HS I had installed the GUI platform, As mentioned in the Hardware setup "Read All registers" option not there, instead of load register option there, but what register…