Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A Hello Team,
Checking with the datasheet of the device the pin39 description is NC together with other pins:
However, checking with the datasheet pin39 is connected to ALARM (LED3), can…
Part Number: MCT8316AEVM Hi, I am analyzing the different output signals of the "MCT8316AEVM".
Is there a DACOUT / SOX output or an other channel to display the switching point during the startup phase from forced commutation to BEMF (sensorless…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A Hello, I have a problem with rotating motor using MCT8316AEVM. I was able to drive a motor with analog input and I2C input modes. However, I could not start rotating a motor with PWM input…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A Hi
Is the IC mounted on the MCT8316AEVM an MP(Mass Production) product? Or is it a sample product?
Best regards, Sasaki
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A , MCT8316Z Hello, I am trying to spin up a small low power motor with the MCT8316AEVM. The motor does not seem to spin up with default settings on the board and the tuning does not seem…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A , MCF8316A Hi Team,
I rotate a motor using external PWM signal. I usually rotate the motor as follows: 1. Turn on power supply, 2. Connect USB cable, 3. Load registers, 4. Disconnect USB…
Part Number: MCT8316AEVM Hello Team,
I'm posting on behalf of my customer:
We use MCT8316AEVM. I set SPEED_CONST in Register MAP as "Speed_Loop" to rotate a motor at constant speed regardless motor load. But, it takes time to reach an intended speed…
Part Number: MCT8316AEVM Other Parts Discussed in Thread: MCT8316A
Hi,
For LED D6, changing the Baud Rate of serial communication will change the way it shines. I would appreciate it if you could tell me what each of them shows.
When the recommended…
Hi Jimmy,
Closing this thread - please let us know if you need further assistance, and help mark the answer from Vishnu as 'resolved' if it answered your question. Thanks!
Best Regards, Andrew
Part Number: MCF8316AEVM
Hi support team.
I had a question regarding GUI from my customer.
We followed the setup steps shown in the GUI and found that when I clicked the settings button shown in the figure below, Fault was detected and the motor could…