Part Number: DRV8312 Other Parts Discussed in Thread: MCT8316Z , MCT8316A , MCF8316A , DRV8316 , DRV8329 , DRV8328 , DRV8300 , DRV8306 , MCT8316Z-Q1 We are required to drive a 3 phase 24V, 3.1A BLDC motor. It is a sensored motor with hall effect sensors built…
Part Number: DRV11873 Other Parts Discussed in Thread: DRV10982-Q1 , DRV10983-Q1 , MCT8316Z-Q1 Hi team
Could you help give an automotive device with similar spec to DRV11873? My customer chosen DRV11873 on a prototype board and now the customer needs a automotive…
Part Number: MCT8316Z-Q1 Other Parts Discussed in Thread: MCT8316Z , MCT8316ZTEVM , DRV8316REVM Hi,
can internal buck converter or AVDD output in MCT8316Z be used for powering external support microcontroller without external nSLEEP pin control? On MCT8316Z…
Part Number: MCT8316ZTEVM Other Parts Discussed in Thread: MCT8316Z , DRV8316-Q1 , MCT8316Z-Q1 Hello,
I am testing this eval with the SPI variant of the chip and I was wondering what the Brake Mode field is used for? Like does it apply a COAST whenever the…
Part Number: DRV8305 Other Parts Discussed in Thread: DRV8306 , DRV832X , DRV8343-Q1 , MCT8316Z , MCT8316Z-Q1 , DRV8304
e2e.ti.com/.../3963447
Sorry I have to come back on this thread that was locked now, due to me taking long. But I need it again.
"..…
Other Parts Discussed in Thread: MCT8316Z , MCF8316A-Q1 , MCT8316Z-Q1 , MCT8316A-Q1 , MCT8316A , MCF8316A Hi team,
My customer is asking whether we have such proper motor driver device with such features for their seat ECU application:
Support 12V supply voltage…
Hi Ruixin,
If the customer needs high accuracy of the motor position and cannot let the motor spin quickly at startup then a non-sensored solution may not be the best device. For low speed solutions that cannot have the startup have higher speeds we recommend…
Other Parts Discussed in Thread: DRV8316 , DRV8316REVM , MCT8316Z , MCT8316Z-Q1 , MCF8316A , MCT8316A , DRV8316-Q1 The DRV8316 and MCx8316 families of 3-phase integrated MOSFET BLDC motor drivers include an up to 200-mA adjustable buck regulator capable of outputting…
Part Number: DRV8306 Other Parts Discussed in Thread: DRV8340-Q1 , MCT8316Z , DRV10983-Q1 , DRV8305 , DRV8305-Q1 , DRV8343-Q1
Do you have an automotive version of DRV8306? If not do you have a part that has a similar function as DRV8306 but is automotive…
Part Number: DRV8311 Other Parts Discussed in Thread: MCT8316Z , MSP430FR2000 , MSP430FR2111 Hi team,
I’ve got two questions on DRV8311. Could you please take a look below, and help me understand this device more?
Q1: In my understanding, DRV8311H…