Part Number: MCT8329EVM Hello,
Our custom solution utilize a 560KV, 14-pole, 12-slot outrunner motor for an automotive application. It is a non-continuous duty application where the system will run at intervals for no more than 30 seconds. The power…
Part Number: MCT8329EVM Other Parts Discussed in Thread: MCT8329A , I'm trying to use MCT8329A with ESP32 S3 and the ESP32 is to send PWM to control the motor speed. I have removed all the jumpers on J9 to disconnect the on-board MSP430.
Can anyone…
Part Number: MCT8329EVM Tool/software: Hello,
I am using MCT8329EVM and I was tuning my brushless motor with adjusting some register...
Since yesterday i can't access to register, i get connection issue when i tried to read register. I can connect…
Part Number: MCT8329EVM Hello,
I am trying to drive a motor (may be a Nidec 42F series) max rpm 3600, operating current 1.1 A, 10 poles with the MCT8329EVM. Following the tuning guide I end up in either Abnormal Speed or LOS fault even if I use the…
Part Number: MCT8329EVM Other Parts Discussed in Thread: CSD18540Q5B
Tool/software:
Hi,
I want to redesign the MCT8329EVM using smaller package MOSFETs . Can someone guide me on how to select appropriate MOSFETs for this design? Are there any calculators…
Part Number: MCT8329EVM I noticed on the Essential Controls page of the Guided Tuning Settings there is a drop down for "Recommended Default Values". The title says to choose an application type but there is nothing on the pull down menu to choose. Is…
Part Number: MCT8329EVM Other Parts Discussed in Thread: MCF8329HS , MCT8329A , I noticed on the Essential Controls page of the Guided Tuning Settings there is a drop down for Recommended Default Values. The title says to choose an application type but…
Part Number: MCT8329EVM Hi Experts,
I bought the MCT8329EVM Evaluation Module and am trying to run a BLDC motor with an external PWM. On the board, I found EXT_SPEED test point so connected a wire from it to my microcontroller ESP32-S3 and ground pins…
Part Number: MCT8329EVM Other Parts Discussed in Thread: MSP430FR2355 , , MSP-EXP430FR2355 , UNIFLASH Tool/software: Hello
I am using eval board MCT8329EVM and i tried to flash the MSP430FR2355 with MSP-EXP430FR2355 board
I can flash the MSP430 inside…
Part Number: MCT8329EVM Tool/software: Hello,
I would like to enable Speed Loop and do the PI Tuning using MCT8329EVM and dedicated GUI.
There is such note in GUI:
How to find this and do the Tuning?
Also this is not working for me (I chosen…