Part Number: MMWAVE-L-SDK Other Parts Discussed in Thread: IWRL1432BOOST , IWRL1432 Hello everyone and TI Experts ,
I am using the IWRL1432BOOST with the MMWAVE-L-SDK (based on the Bike Radar/BSD demo) to develop a long-range detection application …
Part Number: MMWAVE-L-SDK Other Parts Discussed in Thread: IWRL6432AOPEVM , IWRL6432 Hello Team,
I am using the IWRL6432AOPEVM with MMWAVE-L-SDK 05.05.04.02 and the IWRL_Classification_MidBw human/non-human classification demo.
My goal is to detect…
Part Number: IWRL6432AOP Other Parts Discussed in Thread: MMWAVE-L-SDK We’re using MMWAVE-L-SDK Ver. 05.05.04.02 (the latest available).
In file: SDK\source\datapath\dpu\rangeproc\v0\rangeprochwa.c
In function: rangeProcHWA_ParseConfig() at line 1548…
Part Number: IWRL6432AOP Other Parts Discussed in Thread: MMWAVE-L-SDK , Hi,
I'm adding crash-recovery (watchdog + HardFault handling) to an IWRL6432AOP application on MMWAVE-L-SDK 05.05.02.00 / FreeRTOS. Two separate questions:
1. How do I provide…
Part Number: MMWAVE-L-SDK Other Parts Discussed in Thread: IWRL6432AOPEVM I’m looking for a configuration setup that can perform both zoning and human/non-human classification simultaneously.
I have uploaded two config files:
'zone_detection.cfg'…
Part Number: MMWAVE-L-SDK Other Parts Discussed in Thread: IWR6843ISK , MMWAVEICBOOST Thank you for your help. My name is Niwa.
Regarding the following product I purchased from your comapny,
Icreated the case using a 3D printer,
and I would be happy…
Part Number: MMWAVE-L-SDK Other Parts Discussed in Thread: AWRL1432BOOST Dear Engineers,
I currently work with the mmWave_L_SDJ_05_05_04_02 and a AWRL1432BOOST.
When I try to view older measurments using the "PlayBack from Log" button, I can select…
Hello Zigang, Thank you for your response.
zigang Yang said: Is C0 with TX1 + TX2, and C1 with TX1 - TX2?
This is correct yes. C0 is configured with TX1 + TX2, and C1 is with TX1 - TX2. In the LUT i have given 0x33 for the bpm enable. Are these configurations…
Part Number: MMWAVE-L-SDK-6 Other Parts Discussed in Thread: AWRL6844 Hello Team,
We just looked into the range process algorithm and how the radar cube is filled.
Based on the current configuration, it appears that data from only one TX antenna is…
Part Number: MMWAVE-L-SDK Tool/software: I have a question regarding the MMWAVE-L-SDK version 5.5, specifically concerning the Flash submodule within the Board Peripheral Drivers. In the function Flash_eraseSector defined in flash.c, I noticed that a…