The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Part Number: MPY634 Tool/software: Hi team,
Customer wants a MULTIPLIER, one input is 12V and another is 1V. Could you please recommend the best fit?
Nison
Part Number: MPY634 Could someone please provide me with the MPY634 library file? I can't seem to locate it. I'm grateful.
mail id--> eey227533@iitd.ac.in
Part Number: MPY634 Other Parts Discussed in Thread: OPA564 , TINA-TI Hi, I am using MPY634 as a signal conditioning of my DAC output.
I am using the MPY634 in the Basic Multiplier Connection, as the datasheet shows. I connected X1, Y1, and Z2, each to…
Part Number: MPY634 Hello
i'm using the MPY634 mixer chip for making Lock in amplifier.
To configure MPY634's SF(Scale Factor) to 1, I configured the circuit as below.(MPY634 datasheet figure 1.)
However, looking at the resulting values, it doesn…
Part Number: MPY634 Hello
I am using MPY634 IC chip for mixer purpose. And we want to supply +15V and -15V as power.
I have 3 questions
1) How much current limit should I put on the power supply? 2) And how much current is supplied to the power supply…
Part Number: MPY634 Hello
I'm using MPY634 mixer chip
As shown in the picture below, the power pins(15V/-15V) are connected to the power supply and only the ground is connected to the x2 y2 pins, but an internal short has occurred between the input…
Part Number: MPY634 Hello
I have a question about mpy634 frequency range.
Can I use MPY634 about frequency range 1.6Khz~0.1Hz?
If not, Can you recommend another IC chip?
Thank you.
Part Number: MPY634 We wanted to replace the AD734 of ADI, and we don't know if the MPY634 has a typical application circuit that achieves square sum, open root, and rms.
The following diagram is a typical application circuit for the AD734, can we…