Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: ENERGIA Hi there, im pretty much starting from the scratch when it comes to MCU's and programming. At the moment Im playing around with my MSP-EXP430FR6989 and a simple DHT22 reading temp.…
Part Number: MSP-EXP430FR6989
Hi all! My quistions are:
How can I be sure, that this function doesnt end up as a infinite loop?(For example if mathTemp is always smaller than "12", AFE dac value always smaller than 1600?)
What is the "12"…
Part Number: MSP-EXP430FR4133 Other Parts Discussed in Thread: MSP430FR4133 , MSP430FR6989 Tool/software: Code Composer Studio Hello,
I'm traying to use SPI interface to communicate EXP430FR4133 and EXP430FR6989. I used the demo code: msp430fr413x_euscia0_spi_10…
Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: MSP-FET , ENERGIA Tool/software: Code Composer Studio Hi
I have this issue with code composer :
Error initializing emulator: A firmware update is required for the MSP430 Debug Interface (MSP…
HI,
I'm not familiar with the TI-RTOS SDcard example. Have you tried the example as-is without modification on a LaunchPad? Per the example instructions, it uses SPI0. I will suggest you run as is and make sure it works on the LaunchPad. This way it…
Part Number: MSP430FR6989 Other Parts Discussed in Thread: MSP-EXP430FR6989 Can someone help me using the MSP-EXP430FR6989 board and the MSP-FET430UIF programmer using SPIWIRE?
Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: MSPWARE , ENERGIA Tool/software: Code Composer Studio Hi,
I bought a MSP-EXP430FR6989 launch pad and wanted to implement a couple of capacitive touch buttons to control it. It was not my focus…
Hi Mayank,
The TCAN4551-Q is a reduced feature variant of the TCAN4550-Q1 and the TCAN4550 Demo Software is compatible with the TCAN4551-Q1. You can download this demo software from the TCAN4550-Q1 product folder , or from this link .
This demo code was…
Part Number: MSP-EXP430FR6989 Other Parts Discussed in Thread: FLOWESI-GUI , MSPWARE , MSP430FR6989 , EVM430-FR6989 Hi all!
I am working on a water meter and I would like to achive rotation detection / read rotation disk. I would like to count the amount…
Part Number: MSP-EXP430FR6989 HEllo,
I'm trying to get a PWM out on P2.2 using Timer B. The timer won't start counting: Am I setting this up right?
void PWMsetup(void)
{ // Configure GPIO P2DIR |= BIT2; // P2.2 as PWM output P2SEL0 |= BIT2; /…