Hello O.H.,
Windows XP and the MSP-FET430PIF programmer are no longer supported and have not been supported for some time. Please see section 4.1 of the MSP Debuggers User Guide for any available information about the MSP-FET430PIF.
Part Number: MSP-FET430PIF Tool/software: Code Composer Studio Dear Sir
I have this old tool (msp-fet430pif) and using lpt to usb convertor I want to use it with ccs 8 (win 10) to develop msp430g2553 implementation. I see that that win 10 recognize th…
Dear all,
Does the old MSP-FET430PIF support MSP430AFE?
I have a customer encountered problems using them together.
The MSP430 Hardware Tools UG doesn't mention AFE devices. The only point mentioned is that FET430PIF support devices before 2011 including…
Other Parts Discussed in Thread: MSP430F2410 Dear All,
I am working on a system that has MSP430F2410 and I am using the 4-wire JTAG with MSP FET430PIF parallel port programmer. Please let me know if this debugger can be used with Code Composer Studio…
The FET requires a firmware update if it shall support a new MSP. It needs to 'know' the MSP (it's details such as the itnernal flash controller, default timings etc.) If the FET firmware does not know an MSP, it cannot program it.
There is…
The "Smart RF Studio" program is a very useful tool for testing a hardware before loading a custom firmware into it. It is on the one hand.
On the other hand, the useful thing is if the program works with a simple budget license free interface…
Other Parts Discussed in Thread: MSP430F2013 hi, i want to program the MSP430F2013 using MSP-FET430PIF , i have made connection as shown below, is it correct??
i read in the manual of experimental board(MSP430 FG4618/F2013) that msp430F2013 can be programmed…
Other Parts Discussed in Thread: MSP-FET I have a very old parallel port MSP430-FET430PIF. It is still working great with Windows XP. Recently one of the XP machine has gone South so I bought a new one with Windows 7. Now the system fails to download and…
Other Parts Discussed in Thread: MSP430F2112 Hello.
I am using MSP430F2112, while code downloading & debugging
2-Wire Spy-Bi-Wire Communication works fine with MSP-FET430UIF (USB) & debugging works well, but when using MSP-FET430PIF (Parallel Port…
Thanks for trying to help Ethan! I have tried both Chromium (I'm on Ubuntu 20.04) and Firefox. Both seem to fail, but Chromium is telling me I still have an issue with my Cloud Agent Installation, which is at least a little more than Firefox was telling…