Other Parts Discussed in Thread: MSP-FET Hello,
I'm in the process of trying to flash a microcontroller in Code Composer Studio 6. When I'm debugging the code, I get the following message:
Error initializing emulator: A firmware update is required…
Other Parts Discussed in Thread: MSP430FG439 In an application I need to send data to a PC wirelessly.The main unit consist of MSP-FET430U80 target board featuring MSP430FG439 micro controller.I thought of sending the data first to ez430-RF2500 target…
I purchased a TI MSP-FET430U80 (Target board + USB
flash emulation tool). I never could run it. It recognizes the UIF, but it does
not communicate with the microcontroller.
I did install the driver and checked the device manager for proper
installation…
Part Number: MSP430FG439 Tool/software: Code Composer Studio Dear team,
My customer want to measure the frequency of ext signal with timer capture mode.
Hardware: MSP-FET430U80 with FG439
XT1=32.768kHz XT2=4MHz
Code:
#include <msp430fg439.h>
#include …
Hi Gadi,
Sorry for the delayed response.
There shouldn't be any issues using the F2619S for sensor feedback. One thing you will want to consider is to double check that you can achieve the required ADC sampling rate with the F2619S device. Otherwise,…
The MSP430FG437 Product Folder has a listing of appropriate platforms for programming this device in the Design Kits & Evaluation Modules section.
In particular, the MSP-FET430U80 is a platform that can be used if you do not have your own target hardware…
Yes , Do I need This http://www.ti.com/tool/ez430-rf2500 http://www.ti.com/tool/msp-exp430g2 http://www.ti.com/tool/msp-fet430u80
Plz I need advise..
Thanks
I have MSP-FET430U80 target board and I want to interface it with the ethernet controller IC (wiznet W5100) along with the required circuitory in order to control my application through a web page.Basically wiznet will host the web page.Can you help me…
Howard Tang said:
I need to buy a MSP430 and it will be mounted on PCB with my power management unit, which type of packaging should I buy?
You will need to select the ideal MSP430 for your application based on your requirements. You will know these…
Hello,
I'm a student at UFMG here in Brasil and I'm looking forward to build the Pulse Oximeter application (slaa274a/458) with the MSP430FG43X microcontroller.
However, I would like to build it using a suitable Dev Kit (and not the stand…