thank you for the application note it will help me understand the h-bridge much better. Also i am using the MSP-FET430U80 development board will that be a problem with the code ? Are there any development board specific differences that i should take…
Hello We use about 50 pcs MSP-FET430U80 for class work. Every different adapter creats a new com port and needs administration rights for driver installation. Is there any way that all 50 adapter use the same com port and there is no new need for driver…
Hi Ramazan,
there's no starter kit from TI (but maybe from an third party); you need to use http://focus.ti.com/docs/toolsw/folders/print/msp-fet430u64.html (for 64-pin package) or http://focus.ti.com/docs/toolsw/folders/print/msp-fet430u80.html for…
Hi,
Thanks for the reply. I was downlaoded this IAR Embedded Workbench Kickstart software from the website which prompted from installed CD. The software descrption as stated below where the GUI without MSP430F4152 device. Any idea for me to download the…
i am using the MSP-FET430U80 80 pin target board , the code is below and stops after the while statement, the flags are IFG1 & OFIFG
void main(void)
{
double f1;
int32_t x;
int32_t y;
WDTCTL = WDTPW | WDTHOLD;
SCFI0 |= FN_4;…
Other Parts Discussed in Thread: MSP430F5525 hi
i am using MSP-FET430U80 to work on MSP430F5525 using ccsv4. this is the first time i have installed this. but i was unable to connect to my target because it is giving an error MSP430: Error connecting…
Or you can see the following app note: http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=slaa280a
To implement this, you will have to build your own board using the board files available with the app note on the above link. The…