Part Number: MSP430F2619S-HT Other Parts Discussed in Thread: MSP-TS430PM64 , MSP-FET Hi,
Can I use www.ti.com/.../msp-ts430pm64 and http://www.ti.com/tool/msp-fet to flash/program MSP430F2619S-HT? If not what options do I have?
Regards,
Bezak
Part Number: MSP430F417 Other Parts Discussed in Thread: MSP-TS430PM64 I'm doing some testing with the MSP430F417 with the board MSP-TS430PM64. In the LPM3 the current consumed is around 50uA. Is this value correct?
I am measuring the current with…
I also tried it on MSP430F2418 using MSP-TS430PM64 and it worked on my side too.
Note that the Rocket uses different pins (TCK instead of TEST) to generate the entry sequence. I used the BOOTST connector with R6 and R7 on.
Regards,
Luis R
Hi Gadi,
Sorry for the delayed response.
There shouldn't be any issues using the F2619S for sensor feedback. One thing you will want to consider is to double check that you can achieve the required ADC sampling rate with the F2619S device. Otherwise,…
Hello,
Unfortunately, I could not duplicate your issue. Using CCS v8.1.0, I created a new project with 'main.c' for the MSP430F135, copied in your code, saved the project, then downloaded/debugged using a MSP-FET and the MSP-TS430PM64 target board. After…
Hi,
The target board ( http://www.ti.com/tool/msp-ts430pm64 ) can be used for the device debug. From the target board schematic, the pin2 of the JTAG 14 pin connector should be powered. So please change the R4 to 0-ohm and populated. R3 can be no stuff…
I'm quite sure you've got this right. What I would recommend though, if possible, is to experiment before you spin a board. It might save you a lot of heartache. The MSP-TS430PM64 is a pretty nifty development board for those particular chips …
Hi,
Please see the "Description" section on the MSP-TS430PM64 product page. Unfortunately, that target board does not work for MSP430F41x2 devices. Please use the MSP-TS430PM64A target board for the MSP430F4152 instead.
Regards,
Nathan
Баг определения микроконтроллера.pdf The client've made an experiment using of MSP-TS430PM64 Rev1.1 board and MSP430F2617TPM controller, MSP-FET. See attached file. MSP430Flasher defined MSP430F2617TPM as MSP430F2618. What is the reason of the problem may…