Part Number: MSP430F6638 Other Parts Discussed in Thread: MSP430WARE , MSP-FET , MSP430F5529 , UNIFLASH , MSP-TS430PN80USB Hello, My result was the same as the original thread. In my case the TGT part# was F6638 which came with the EVM.
Findings:
"Unknown USB…
Part Number: MSP-TS430PZ100USB Tool/software: Code Composer Studio OS: XP
CCS version: v5.3
Device: MSP-TS430PZ100USB of the MSP430F5636 and MSP-FET430UIF
Hello,
I recently using MSP-FET430UIF programmers for my device, my code uses " Blink The LED " in CCS…
Part Number: MSP430F6633 Other Parts Discussed in Thread: MSP430F5529 , MSP-FET Dear Team,
I'm facing issue while running USB CDC Virtual COM port C1_LedOnOff example on MSP-TS430PZ100USB board (Rev 1.25) with MSP430F6633 (Rev E). It says Unknown USB…
MSP430F5659 and MSP-TS430PZ100USB Target Board
We have One piece of Start up code that NOW deals with any XT2 Crystals 4-20 MHz and XT1 32.768KHz.
The problem was absolutely NOTHING to do with previous suggestions.
I have changed position and happy…
Part Number: MSP430F5632 Hi Team,
Can you please help us with our customer's inquiry below.
I have got the H3_EchoToHost working on www.ti.com/.../MSP-TS430PZ100USB launchpad using MSP430F5632 mc and I added function to communicate over uart on port…
Hello Experts,
Good day.
The system that did not work never had IAR, Eclipse, CCS, Elprotronics, or anything like that installed.
This process is to be used by production staff, not developers, so no compiler, IDE or debugger of any kind is being used…
Other Parts Discussed in Thread: MSP-FET Bonjour
Je commande une carte de developement msp-ts430pz100usb mais je ne l'avais pas compris que je besoin d'un outil de débogage trop. Quelqu'un pourrait-il me dire ce que MSP-FET choisir parce…
English is fine ;). I have several peripherals connected to the MSP-TS430PZ100USB: The AD7490EVKIT which is powered externally by a 12V SMPS, which makes a very chep impression to me, and a MAX14502EVKIT which is also powered by my USB port. At the beginning…
Hi,
I want to program the TI's MSP-TS430PZ100USB through it USB port, but I am not able to program it. It is not getting detected even after installing the drivers. Please help me out.