Hello Peter,
Thanks for sharing the customer's feedback and for digging. While the MSP-TS430RHB32A target socket board will accept 32-pin QFNs, the pin connections won't match up with the QFN package of the MSP430F2122 device, so they won't be able to…
Part Number: MSP430I2020 Other Parts Discussed in Thread: MSP-TS430RHB32A
Tool/software: TI C/C++ Compiler
Test condition:
- MSP-TS430RHB32A board
- GAIN 1
- Measuring result = 10 data average
- sample program "sd24_ex4_singleConversionSingleChannelPolling…
Part Number: MSP430I2020 Other Parts Discussed in Thread: MSP-GANG , , MSP-TS430RHB32A Hello,
My customer can not write to Flash Memory that using MSP-GANG programmer.
The combination they're using.
PC - USB - MSP-GANG - Splitter - (MSP-TS430RHB32A…
If the MSP430 still fails with the basic code then this verifies a power supply or hardware issue. Can you please capture some screenshots of VCC, VCORE, and RST lines during a disturbance which crashes the MCU? Are you able to share any PCB design…
Hi Fran,
You were having a problem with the backchannel UART on the MSP-FET, when running the code example msp430i20xx_euscia0_uart_01.c completely unaltered, correct? I just tried running this example on a TI target board, and it worked with the MSP…
Hi Ryan,
I did a quick experiment in TI eval board MSP-TS430RHB32A
The board has provisions for pull-down (10K) to gnd the A+ and A-. When the the ADC is converting, you can observe a 100mV 10mV on the resistor on A+. Seems the input is acting as a 1uA…
Hello Chris,
The MSP430-FLASHER log indicates that the MSP-FET firmware and drivers are up to date and that there is successful communication between the FET and target MSP430i2041 device. The MSP flasher supports .hex files and 0x8000 is the correct…
Bina,
This is a mistake in the MSP430I2030's tools software page that I am currently working to have corrected, rest assured that the MSP-EXP430G2 LaunchPad is incompatible with all MSP devices outside of the MSP430G2xx2, MSP430G2xx3, and MSP430F20xx…
Other Parts Discussed in Thread: MSP-TS430RHB32A , MSP430I2020 , MSP-FET , MSP-EXP430FR6989 CCS hangs quite often while I'm trying to build my code. There's a "Configuring Debugger" pop-up that says "Initializing MSP430 (Cannot be canceled)" but nevertheless…
Other Parts Discussed in Thread: MSP-TS430RHB32A Hi,
In my measurement of boot current with MSP-TS430RHB32Aand battery, the current consumption is over 10.0mA. And the execute S/W is simle blinky hex code. Off course whe measure the current ,remove Jumper2…