Other Parts Discussed in Thread: MSP430AFE252 , MSP-FET I am having problems debugging an AFE part when using a G2 Launchpad (V1.4 = old) (As previously described - e.g. "MSP430AFE252 and debugging issues" thread)
Device will program and step through…
Other Parts Discussed in Thread: MSP430AFE252 hii
i am using msp430afe252 for my energy meter application.can any one tell me how i should have 1 second duration frame in which the current or voltage samples are to be calculated.
Other Parts Discussed in Thread: MSP430G2553 , MSP430AFE252 , MSP430WARE hello ,
i want to interface msp430afe252 with msp430g2553 via spi ....
please help me with the code...i want to use 3wire spi mode
as i have only one slave....
Other Parts Discussed in Thread: MSP430AFE252 HIII,
FOLLOWING IS THE SIMPLE LOOPBACK PROGRAM FOR SPI.
BUT I CAN NOT HAVE THE DATA IN RXBUF.
I M USING MSP430AFE252 IN SLAVE MODE
#includemsp430afe252.h unsigned char MDATA; void main(void) { volatile unsigned…
Other Parts Discussed in Thread: MSP430AFE252
I am bounding through all the hoops to upgrade from CCSv4.2 to v5.1 .
My MSP-FET430UIF is v1.4a.
I am debugging an MSP430afe252 device.
Upon import of the CCSv4.2 workspace, the debugger requested…
Other Parts Discussed in Thread: MSP430AFE252 Hi all,
I have an application using an MSP430AFE252. The MSP430 spends most of its time (ideally) in LPM4. When awakened via a GPIO interrupt, it must begin reading an analog waveform using the SD24 ADC as…
Other Parts Discussed in Thread: MSP430AFE252 , MSP430AFE253 Hi,
I'm using the MSP430AFE252 (4MHz), and using the two ADCs to measure two input differential voltages and also measure the temperature sensor.
The problem I'm having is that the temperature…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…