Dear Jens-Michael Gross,
Thanks for your reply.
Previously i have used the MSP-FET for MCU : MSP430F1122 and i have loaded many programs in
MSP430F1122 MCU by using Launch PAD : MSP-TS430PW28
Now I have changed my MCU : MSP430G2230
Also changed Launch…
I am working on : MSP430F1122 Controller.
Launch Pad : MSP-TS430PW28 Texas Instrumentation Launch Pad.
I am giving giving falling edges within interval of 6 milli seconds, so if any delay by SCS bit it will be tolerable.
Regarding giving edges, i have verified…
Other Parts Discussed in Thread: MSP430F1122 Device: MSP430F1122
Programming tool: GANG430
Programming software:MSP-GANG430
Target connected: 1
Hi, i am going to write an unique serial number into the information flash at @1000&1001, i have gave ti…
Thank u aBUGSworstnightmare,
This is the problem due to the li mited time available,there is no time to make new PCBs.So it should be Launch pad and F2012 .I am trying with EZ430-RF2500T - MSP430 2.4-GHz Wireless Target Board.But this is not sure since…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
hey, thanks for your reply
but i forgot to mention that i dont have the normal input board.. i have a old one named "input-ir board" so no usb and no gui.. only a msp430f1122 that i have programmed to control the tas5518
and i do have sound, only…
Other Parts Discussed in Thread: MSP430F1132 , MSP430F1232 , MSP430F2232 , MSP430F2274 , MSP430F1122 , MSP430F1222 Hi,
in my latest project I'm working with an MSP430F1132. Now I'm facing a strange problem when I try to debug my code! An error message shows…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…