Other Parts Discussed in Thread: MSP430G2452 , MSP430F1132 I have a program which works fine in a MSP430F1132 part but fails to work when migrated to a MSP430G2452 part. Both parts should be functionally the same as they have the same set of peripherials…
Hello peg!
You're right, bsl entry of MSP430F5418A or MSP430F5435A is possible using inverted TEST signal sequence! It's like bsl entry of the MSP430F1132 microcontroller.
I've tried this method on my MSP430F5418A and MSP430F5435A - bsl…
Hi Phil,
is the error somehow like the one I've posted here for MSP430F1132 ( http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/39942.aspx )?
Rgds aBUGSworstnightmare
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave