Other Parts Discussed in Thread: MSP430F1222 I am taking some existing PIC 'C' code and coverting to MSP430 using CCE. I have run into the following problem:
#define MAXLINES 50
char *W[MAXLINES]; //array of pointers
The linker does not like the…
Other Parts Discussed in Thread: CC2420 , MSP430F1222 , SIMPLICITI Hello Everybody,
I’m using the CC2420 for a wireless application. But I’m having trouble with the communication between two nodes (One is a MSP430F1222 and the other is a PIC Micro PIC18F4685…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
Other Parts Discussed in Thread: MSP430F1132 , MSP430F1232 , MSP430F2232 , MSP430F2274 , MSP430F1122 , MSP430F1222 Hi,
in my latest project I'm working with an MSP430F1132. Now I'm facing a strange problem when I try to debug my code! An error message shows…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
Hello Pavel,
EDIT: I didn't read past your first error. You already did this, and I didn't notice.
Pavel Hristov said:
We tried adding the following lines in io.h
#elif defined(__ MSP430F6726 __) #define __MSP430_6726__
For your first error, you…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited by…